Difference between NFC Reader Library for PN5190 and Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Difference between NFC Reader Library for PN5190 and Linux

2,989件の閲覧回数
ttkk_01
Contributor I

Hello.
I want to know the difference between NFC Reader Library for PN5190 and Linux.
The latest library version is following
- for PN5190: v07.05.00
- for Linux: v07.03.00

If I want to develop in Linux environment, does it need to use v07.03.00?
If Yes, is there any risk about not using v07.05.00, and how to support PN5190 FW v2.05?
(It looks for Linux doesn't support PN5190 FW v2.05)

0 件の賞賛
返信
3 返答(返信)

2,973件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi @ttkk_01 

 

pleaser refer to the revision difference

danielchen_0-1663302101437.png

The new features in Reader Library v7.05 is related with PN5190 firmware 2.05.

I would suggest you start with Read library v7.03 , and merge the new features in v7.05 into your project,    then you can use PN5190 v2.05.

I will ask internally when the reader library v7.05 for Linux will be ready. 

 

Regards

Daniel

 

 

Regards

Daniel

 

 

 

0 件の賞賛
返信

2,944件の閲覧回数
ttkk_01
Contributor I

Hi @danielchen .

OK understood.
I will try to start with Reader Library v7.03 and PN5190 v2.03.
And after released, replace updated one.
Did you get information about v7.05 for Linux?

0 件の賞賛
返信

2,941件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

it is not ready. I will keep you informed.

 

Regards

Daniel

0 件の賞賛
返信