DESFire Light Symmetric Originality Check

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DESFire Light Symmetric Originality Check

3,115件の閲覧回数
wilmer_suarez
Contributor III

Hello,

I'm working on implementing the necessary LRP algorithms to perform Symmetric Originality Checks on DESFire Light. I'm following the information available in AN12343 and AN12304. I understand the use of an AES key as an input to the precomputation functions is needed. This makes sense when authenticating with any of the internal Application Keys.

However, I don't understand how this works with the Originality Keys. These key are unique to every DESFire Light card, correct?

How do I obtain the Originality Keys?

Are they the same as the Application Keys, as in you can change them?

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

3,096件の閲覧回数
wilmer_suarez
Contributor III

@Kan_Li Hi, thank you for your response. I currently have a valid NDA on my docstore account. I am unsure where and what to look for in the docstore to find this information. Do I submit a support e-mail?

0 件の賞賛
返信

3,077件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @wilmer_suarez ,

 

Yes, please create a private ticket attached with your valid NDA according to the following link.

https://community.nxp.com/t5/Using-Our-Community-Knowledge/How-to-submit-a-new-question-for-NXP-Supp...

 

Thanks for your patience!

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

3,100件の閲覧回数
Kan_Li
NXP TechSupport
NXP TechSupport

Hi @wilmer_suarez ,

 

Please kindly refer to the following for details.

 

These key are unique to every DESFire Light card, correct?

- Yes, they are.

 

How do I obtain the Originality Keys?

- This kind of information should be requested from the NXP docstore with a valid NDA, so please contact your local Disty or NXP sales representatives to sign the NDA at first. You may refer to https://www.nxp.com/support/sample-and-buy/distributor-network:DISTRIBUTORS for more details.

 

Are they the same as the Application Keys, as in yoYpou can change them?

- No, they are not. According to the spec,  

• The keys are written on the IC at the production in the NXP factory.
• Keys are created in NXP factory HSM and never leave the secure environment.
• The keys can`t be changed after the IC leaves the NXP factory.

 

Hope that helps,

 

Have a great day,
Kan


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

 

 

0 件の賞賛
返信