DESFire EV3 Formatting Issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DESFire EV3 Formatting Issue

5,785 Views
Riowang-Akuvox
Contributor II

The issue we are encountering is as follows: When using a DESFire EV3 8K card, after sending the 0xFC format command to format the card, the card enters a "frozen" state and does not respond to any further commands. Even removing the card from the field, re-scanning it, or re-running the code does not resolve the problem. However, we found that when the card is read by a smartphone's NFC function, it recovers and can execute other commands normally. The problem reoccurs as soon as the card is formatted again.

Additionally, we tested several other DESFire cards. Three of the EV1 cards exhibited similar issues, while the three EV2 cards and two EV3 cards worked normally after formatting.

This situation suggests that after the card is formatted, it does not return to its normal operating state. However, when the card is read by a smartphone's NFC function, it seems to reactivate and return to normal operation. The strange thing is that only certain DESFire cards exhibit this behavior.

Tags (2)
0 Kudos
Reply
8 Replies

5,174 Views
NeatCar
Contributor I

I'm having the same problem with EV3 cards after command 0xFC. I'm using a custom NFC reader with custom firmware. It works perfectly for all EV2/EV3 commands so far, except for this one.

Steps to reproduce:

  1. Bring card into RF field.
  2. Card is discovered.
  3. Send GetVersion command (0x60). Response is good.
  4. Select application 0x000000.
  5. Authenticate with PICCMasterKey. Success.
  6. Send command 0xFC. NO RESPONSE.
  7. Remove card from RF field.
  8. Bring card back into the RF field.
  9. Card is discovered.
  10. Send GetVersion command (0x60). NO RESPONSE.
  11. Repeating steps 7-10 always has the same result.
  12. Reading the card with an Android NFC phone "fixes" the card. Now it responds to GetVersion.
0 Kudos
Reply

5,756 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @Riowang-Akuvox 

From your description, formatting failed. At PICC level, all applications and files are deleted by Format(0xFC) command,but before that, you must authenticate the card, and successed, and then you can format the application and files.

0 Kudos
Reply

5,754 Views
Riowang-Akuvox
Contributor II
Yes, as you mentioned, I’ve already authenticated the PICC before formatting, and based on the read results, the formatting has indeed been completed (all created applications are deleted). However, the issue I’m encountering now is that after formatting, the card cannot execute other commands. For example, commands like selecting an application, authentication, and getting the version all fail. But after reading the card with a phone’s NFC function, when I put the card back on the reader, it works normally.

This issue seems like the card isn’t restored to the correct state after formatting, while reading it with a phone’s NFC function somehow reactivates it to a normal state. What’s odd is that this issue only occurs with one EV3 card and a few EV1 cards I have, while other cards (EV1, EV2, or EV3) work fine with formatting, application creation, or file creation.
0 Kudos
Reply

5,738 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @Riowang-Akuvox 

After formatting, you need to reset your reader and then re-active layer3/4 ,and then create the new application and file, please try.

0 Kudos
Reply

5,723 Views
Riowang-Akuvox
Contributor II
Thank you for your response. As you mentioned, after formatting, I have reset the card reader and re-executed the anti-collision card selection process that complies with the 14443A standard. At this point, reading the 7-byte UID from the Desfire card works normally, but executing Desfire-related commands still fails. I think it’s worth noting that, among the Desfire cards I currently have, only some cards exhibit this issue while others work fine. If there were flaws in our formatting process or workflow, it would likely result in all cards malfunctioning rather than only some. This problem might be due to unknown differences between various Desfire cards. When this issue occurs with one card in my possession, it can also be reproduced with other cards from the same batch. I hope you can provide more information for reference, and I look forward to your reply.
0 Kudos
Reply

5,688 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @Riowang-Akuvox 

Your situation is strange, I have not reproduced your situation, your card is a clone card?

0 Kudos
Reply

5,684 Views
Riowang-Akuvox
Contributor II
Actually, the Desfire cards I have are physical cards that we purchased from a card manufacturing supplier.
0 Kudos
Reply

5,620 Views
KaiLi
NXP TechSupport
NXP TechSupport

Hello @Riowang-Akuvox 

 As the final way, it is recommended to try the NXP Reader CLRD730 (PEGODA Contactless Smart Card Reader | NXP Semiconductors).

0 Kudos
Reply