Complex Logic for Discovery Loop

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Complex Logic for Discovery Loop

1,534 Views
aceviker
Contributor I

Hi, I need to implement a loop where a Layer 4 Type A card with a specific application is selected and any other type of card is ignored. Even if multiple card types or multiple Layer 4 Type A cards are on the reader the reader must select with the Layer 4 Type A with the correct application.

How can i achive this with the discovery loop. 

Labels (1)
0 Kudos
Reply
1 Reply

1,453 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

The discovery loop will only poll for types, the switching to Layer 4 and selection of the correct Tag with specific information shall be carried out on the application side.

Best regards,

Ivan.

0 Kudos
Reply