Can't set Device in pass-through mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can't set Device in pass-through mode

1,479 次查看
markussköld
Contributor I

HI,

I am working with NT3H2111_2211 and developing an app using it. 

I seem to have a problem getting the NC_REG in to the right mode. it keeps giving the value 0x3D and never going in to 0x7D. I have done some debugging and the result is as follows:

- Session Register from Mirrored Session Register (sector 3, block 0xF8)

         - PTHRU_ON_OFF = 1b (value: 64)

         - PTHRU_DIR = 1b (value: 1)

         - FD_ON = 11b (value: 12)

         - FD_OFF = 11b (value: 48)

         - SRAM_MIRROR_ON_OFF = 1b (value: 2)

With this the NC_REG still gives 0x3D...

Any idea where I'm going wrong? Is there any specific issue known that could prevent it to get in to pass-through mode?

Best Regards

Markus

标签 (1)
标记 (3)
0 项奖励
回复
2 回复数

1,373 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please refer to the following Application Note about how to use the pass-through mode:

https://www.nxp.com/docs/en/application-note/AN11579.pdf 

Regards,

Ivan.

0 项奖励
回复

1,086 次查看
wangwenyu
Contributor II

@IvanRuiz 

I have the same problem. I read AN11579 completely. It is not helpful. I can set other bits of NFC_REG. But I can't enable PASS_THROUGH. Even though I repeat to set this bit, it still can't be set.

 

bool bReturn = false;

NTAG_SetTransferDir(ntag_handle, RF_TO_I2C);
NTAG_GetTransferDir(ntag_handle, &bReturn);


NTAG_FD_OFF_FUNCTIONS_T ngat_fd_off;
NTAG_FD_ON_FUNCTIONS_T ngat_fd_on;

NTAG_SetFDOffFunction(ntag_handle,
I2C_LAST_DATA_READ_OR_WRITTEN_OR_RF_SWITCHED_OFF_11b);
NTAG_SetFDOnFunction(ntag_handle, DATA_READY_BY_I2C_OR_DATA_READ_BY_RF_11b);

NTAG_GetFDOffFunction (ntag_handle, &ngat_fd_off) ;
NTAG_GetFDOnFunction (ntag_handle, &ngat_fd_on) ;

do
{
for(ver_num = 0 ; ver_num < 500; ver_num++);


NTAG_SetPthruOnOff(ntag_handle, true);
NTAG_GetPthruOnOff(ntag_handle, &bReturn);
}while(bReturn != true);


// Force the counter to be placed into memory
volatile static int i = 0 ;

0 项奖励
回复