CT & CLIF Card Operation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CT & CLIF Card Operation

3,151 Views
sachin_singh
Contributor II

Hi All,

I am working on the PN7462AU card reader with Evaluation kit using PN7462AU-FW_v05.07.01_Full firmware file with "phExCcid" example. Which is for Contact and Contact-less cards detection.

I need to perform the operation on both card when both are present at same time. But yes only one card get the command fired by the user respectlivily.

For example say that, Card reader has both the card Contact and contact-less card present at the same time. When user need to fire command for contact card then it should received by contact card similarly for the contact-less also. (For Contact-less card - MIFARE CLASSIC 1k and contact card - SAM CARD).

In short I need to perform the operation on both cards (contact and contact-less cards) but one at a time in presence to two cards - contact and contact-less cards.

So, Please kindly guide to achieve these functionality for two card operation on PN7462AU.

If possible then also share the API/data/document/any example related to it.

Your all the support & response are highly appreciative.

Looking forward for the supports.

Regards

0 Kudos
Reply
2 Replies

2,941 Views
hglanzer
Contributor I

hi,

having the same problem as describe by 'sachin_singh'. could you elaborate how to solve this?

thx in advance

hari

0 Kudos
Reply

3,067 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

A reply was already made to your case.

BR,

Ivan.

0 Kudos
Reply