CT & CLIF Card Operation

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CT & CLIF Card Operation

3,223 次查看
sachin_singh
Fresh Out Contributor

Hi All,

I am working on the PN7462AU card reader with Evaluation kit using PN7462AU-FW_v05.07.01_Full firmware file with "phExCcid" example. Which is for Contact and Contact-less cards detection.

I need to perform the operation on both card when both are present at same time. But yes only one card get the command fired by the user respectlivily.

For example say that, Card reader has both the card Contact and contact-less card present at the same time. When user need to fire command for contact card then it should received by contact card similarly for the contact-less also. (For Contact-less card - MIFARE CLASSIC 1k and contact card - SAM CARD).

In short I need to perform the operation on both cards (contact and contact-less cards) but one at a time in presence to two cards - contact and contact-less cards.

So, Please kindly guide to achieve these functionality for two card operation on PN7462AU.

If possible then also share the API/data/document/any example related to it.

Your all the support & response are highly appreciative.

Looking forward for the supports.

Regards

0 项奖励
回复
2 回复数

3,013 次查看
hglanzer
Contributor I

hi,

having the same problem as describe by 'sachin_singh'. could you elaborate how to solve this?

thx in advance

hari

0 项奖励
回复

3,139 次查看
IvanRuiz
NXP Employee
NXP Employee

Hello,

A reply was already made to your case.

BR,

Ivan.

0 项奖励
回复