CLRC66303 for Felica Test

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CLRC66303 for Felica Test

1,284 Views
alexshen
Fresh Out Contributor

Our customer--Spectra Technology(HK) using CLRC66303 will apply Felica cert. in mid-Dec.

 

In digital protocol test, there is a requirement for below two timings.  May I have your suggestion that which registers can tune these two timings?

 

  1. Guard time [Red item]
  2. RF output on to first command. 捕获.JPGThank you!
Labels (1)
0 Kudos
Reply
1 Reply

1,223 Views
IvanRuiz
NXP Employee
NXP Employee

Hello,

As the requirements mention, this has to be set on the application directly. This will be possible through the NFC Reader Library. Unfortunately, these specific requirements are not implemented on the examples but you may achieve it by controlling when the RF field is ON through phhalHw_FieldOn(); API and sending the command after the specified time you require.

Hope this helps!

BR,

Ivan.

0 Kudos
Reply