CLRC66303 for Felica Test

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CLRC66303 for Felica Test

1,247件の閲覧回数
alexshen
Contributor I

Our customer--Spectra Technology(HK) using CLRC66303 will apply Felica cert. in mid-Dec.

 

In digital protocol test, there is a requirement for below two timings.  May I have your suggestion that which registers can tune these two timings?

 

  1. Guard time [Red item]
  2. RF output on to first command. 捕获.JPGThank you!
ラベル(1)
0 件の賞賛
返信
1 返信

1,186件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

As the requirements mention, this has to be set on the application directly. This will be possible through the NFC Reader Library. Unfortunately, these specific requirements are not implemented on the examples but you may achieve it by controlling when the RF field is ON through phhalHw_FieldOn(); API and sending the command after the specified time you require.

Hope this helps!

BR,

Ivan.

0 件の賞賛
返信