CLRC663 NXP NFC Cockpit

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CLRC663 NXP NFC Cockpit

4,764件の閲覧回数
alvinwong1109
Contributor I

I am using CLRC663 evaluation board and try to use this board to read the UID of the tag with ISO15693. I loaded the secondary firmware file(nnc.bin) to the NXP NFC Cockpit, but I failed and the software does not work anymore. I tried to install it again but It still does not work. I think that I have loaded the wrong file to the board. What should I do?

タグ(2)
0 件の賞賛
返信
4 返答(返信)

4,544件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Tsz Tang Wong,

Please flash LPC firmware by refer: Program the firmware to PNEV5180B board
Since you are using CLRC663 evaluation board, the firmware can be found in C:\nxp\NxpNfcCockpit_v4.8.0.0\firmware\Secondary_RC663\BootLoader_And_Nfcrdlib_SimplifiedAPI_EMVCo_Secondary.bin
Then CLEV6630B will be able to connect to Cockpit again.

Cockpit read UID ISO15693.png

Best Regards,

Robin

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

4,288件の閲覧回数
AlanSbor
Contributor II

Good answer!

Realy work.

Thanks a lot!

 

Alexey.

0 件の賞賛
返信

4,544件の閲覧回数
alvinwong1109
Contributor I

hi Robin,

After I flash the LPC FW, it comes to another error and it is still disconnected.error2.png

0 件の賞賛
返信

3,821件の閲覧回数
Supreeth
Contributor I

We Have the same issue... Please some once answer

 

Regards

Supreeth

0 件の賞賛
返信