CLRC663-02 and CLRC663-03 INT Pin

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CLRC663-02 and CLRC663-03 INT Pin

1,769 Views
MikeBrennan
NXP Employee
NXP Employee

I just wanted to confirm that there is no changes between the two revisions on the functionality of the INT pin?


Thanks,
Mike

Labels (1)
0 Kudos
Reply
1 Reply

1,608 Views
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Michael,

   Their INT (IRQ) functions are same.


Have a great day,
TIC  weidong sun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos
Reply