CLRC663-02 and CLRC663-03 INT Pin

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CLRC663-02 and CLRC663-03 INT Pin

1,619 次查看
MikeBrennan
NXP Employee
NXP Employee

I just wanted to confirm that there is no changes between the two revisions on the functionality of the INT pin?


Thanks,
Mike

标签 (1)
0 项奖励
回复
1 回复

1,458 次查看
weidong_sun
NXP TechSupport
NXP TechSupport

Hello Michael,

   Their INT (IRQ) functions are same.


Have a great day,
TIC  weidong sun

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复