Android HCE with PN7150 as reader

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Android HCE with PN7150 as reader

2,116件の閲覧回数
erik_su
Contributor I

Trying to use the PN7150 as a reader that works with Android HCE (host card emulation). Android HCE with Android as a reader works fine with the standard APDU commands, but I don't see any documentation with regards to this for the PN7150. 

Are there any resources or examples on the PN7150 that is helpful for this kind of project? Thanks!

0 件の賞賛
返信
1 返信

1,919件の閲覧回数
IvanRuiz
NXP Employee
NXP Employee

Hello,

Please make sure that the Android device supports the full features of a real card and that it is not only demodulating the carrier as a e.g. type A tag and responding to anti-collision. The PN7150 will have to be treated as a normal Reader/Writer, it is rather necessary to check e.g. the card commands and timings for a proper integration.

Regards,

Ivan.

0 件の賞賛
返信