Active peer to peer mode problem(to. pn532 , Initiator)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Active peer to peer mode problem(to. pn532 , Initiator)

2,244 Views
kimhyungjun
Contributor I

Getting 0x13 error while trying to perform DEP for NFC pn532 in active peer to peer mode.How to solve the same? 

0 Kudos
Reply
2 Replies

2,225 Views
Fabian_R
NXP TechSupport
NXP TechSupport

As you may know, this error has to do with the matching of specifications, if you are using PN532 on both ends please clarify to us which board are you using and if the board does work detecting any PICC.

This is for the sake of discard that the antenna and circuit of the antenna are working properly due to the possibility of getting an Invalid RF received Frame at initiating the transmission.

Please check the PN532 Design Kit for the board specification design.

Also please rectify to us if you are using the SDK P2P test so we can have an entry point to assist you.

Best Regards,
Fabian
0 Kudos
Reply

2,218 Views
kimhyungjun
Contributor I

The device that uses the PN532 V3 MODULE board and communicates with P2P uses the ST25R3911B chip.

Is P2P communication with ST25R3911B?

Is the antenna design of the PN532V MODULE wrong?

 

ATR REQ ATR RES was successful

0 Kudos
Reply