14443 TypeB card reader using PN532

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

14443 TypeB card reader using PN532

ソリューションへジャンプ
2,125件の閲覧回数
tetsuomaeda
Contributor III

Hi, I have a question regarding PN532.

We are designing an NFC typeB card reader using PN532.

Following is the log of the communication between PC and the card reader “IFD” equipped with PN532.

PC -> IFD : INITIATOR : LIST PASSIVE TARGETS
00 00 FF 09 F7 D4 4A 01 01 00 FF FF 00 00 E2 00

IFD -> PC : ?
           00 00 FF 00 00 D5 00

We think that the response from IFD should be ACK,

00 00 FF 00 FF 00

Actually in case of the card reader equipped with PN533, the response was ACK.

Does anyone know the reason why the response is not ACK?

I’d appreciate any rresponse.

Regards,

Tetsuo Maeda

タグ(4)
0 件の賞賛
返信
1 解決策
1,894件の閲覧回数
tetsuomaeda
Contributor III

Hi, All,

We have solved the issue.

Thanks for your interest.

Regards,

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,895件の閲覧回数
tetsuomaeda
Contributor III

Hi, All,

We have solved the issue.

Thanks for your interest.

Regards,

0 件の賞賛
返信