14443 TypeB card reader using PN532

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

14443 TypeB card reader using PN532

Jump to solution
2,124 Views
tetsuomaeda
Contributor III

Hi, I have a question regarding PN532.

We are designing an NFC typeB card reader using PN532.

Following is the log of the communication between PC and the card reader “IFD” equipped with PN532.

PC -> IFD : INITIATOR : LIST PASSIVE TARGETS
00 00 FF 09 F7 D4 4A 01 01 00 FF FF 00 00 E2 00

IFD -> PC : ?
           00 00 FF 00 00 D5 00

We think that the response from IFD should be ACK,

00 00 FF 00 FF 00

Actually in case of the card reader equipped with PN533, the response was ACK.

Does anyone know the reason why the response is not ACK?

I’d appreciate any rresponse.

Regards,

Tetsuo Maeda

Tags (4)
0 Kudos
Reply
1 Solution
1,893 Views
tetsuomaeda
Contributor III

Hi, All,

We have solved the issue.

Thanks for your interest.

Regards,

View solution in original post

0 Kudos
Reply
1 Reply
1,894 Views
tetsuomaeda
Contributor III

Hi, All,

We have solved the issue.

Thanks for your interest.

Regards,

0 Kudos
Reply