Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
KW45 Knowledge Hub KW45’s three-core architecture integrates a 96 MHz CM33 application core, dedicated CM3 radio core and an isolated EdgeLock Secure Enclave. The Flash-based radio core with dedicated SRAM delivers a highly configurable and upgradeable software-implemented radio, freeing resources on the main core for customer application space. The Bluetooth Low Energy 5.3-compliant radio supports up to 24 simultaneous secure connections. The EdgeLock Secure Enclave’s isolated execution environment provides a set of cryptographic accelerators, key store operations and secure lifecycle management that minimizes main core security responsibilities. The KW45 MCU additionally integrates FlexCAN, helping enable seamless integration into an automobile’s in-vehicle or industrial CAN communication network. The FlexCAN module can support CAN’s flexible data rate (CAN FD) for increased bandwidth and lower latency. KW45 Block Diagram KW45 Architecture Block Diagram Documents Reference Manual Datasheet Errata Secure Reference manual** Security Certifications  SESIP Level 2 Cert SESIP Level 2 ST PSA Level 2 Certification Regulatory Certifications RED Certification EUROPEAN UNION DECLARATION OF CONFORMITY (EVK) EUROPEAN UNION DECLARATION OF CONFORMITY (LOC) Japan MIC KW45-LOC _TELEC-20250221 Bluetooth Qualifications Qualified Products | Bluetooth® Technology Website Qualification Workspace - KW45/MCX W71 Bluetooth IInterested in Bluetooth technology? Bluetooth® Low Energy Primer – Essential reading for understanding BLE fundamentals. Bluetooth® Specifications – Full list of standards, protocols, and technical documents. Awards and Recognition - Every year, the Bluetooth Special Interest Group (SIG) celebrates the hard work and commitment of working groups, committee members, and contributors who have been recognized by their peers as making a difference in advancing Bluetooth technology, like NXP! 2024: Channel Sounding 2025: Channel sounding amplitude-based attack resilience, LE test mode enhancements and Ranging profile and service.  Bluetooth AI Assistant - Amber   Bluetooth Feature Overview Bluetooth_5.0_Feature_Overview  Bluetooth_5.1_Feature_Overview  Bluetooth_5.2_Feature_Overview Bluetooth_5.3_Feature_Overview Bluetooth_5.4_Feature_Overview Bluetooth_6_Feature_Overview Bluetooth_6.1_Feature_Overview Bluetooth_6.2_Feature_Overview Bluetooth_6.3_Feature_Overview Bluetooth Core Specification Core Specification 4.0 Core Specification 4.1 Bluetooth 4.1 FAQ Core Specification 4.2 Bluetooth 4.2 FAQ Core Specification 5.0 Core Specification 5.1 Core Specification 5.2 Core Specification 5.3 Core Specification 5.4 Core Specification 6.0 Core Specification 6.1 Core Specification 6.2 Core Specification 6.3 Evaluation boards KW45 KW45-EVK KW45-EVK Schematic KW45-EVK Design Files KW45-EVK User manual KW45-LOC User manual KW45-EVK Getting Started Application Notes Software, Hardware and Peripherals: AN14122 : How to use RTC on KW45 This application note describes how to configure and use the RTC peripheral in a BLE demo AN14141 : Enabling Watchdog Timer Module on KW45 Bluetooth Low Energy Connectivity Stack This application note describes the process to implement the WDOG timer in a Connectivity Stack demo. AN13855 : KW45/K32W1 Integrating the OTAP Client Service into a Bluetooth LE Peripheral Device This Application note provides the steps and process for integrating the Over the Air Programming Client Service into a BLE peripheral device. AN13584 : Kinetis KW45 and K32W1 Loadpull Report This application note describes measurement methodology and associated results on the load-pull characteristics. AN13860 : Creating Firmware Update Image for KW45/K32W1 using OTAP tool This application note provides the steps to create and upgrade the image on the KW45 board via OTAP. AN14077 : Steps to migrating KW45 (1MB) to KW45 (512kB) This application note describes the initial steps require to migrate from 1MB flash to 512kB flash. AN14746 : EEPROM Emulation for the KW45B41Z and K32W148 This document describes the process for the EEPROM emulation for the KW45B41Z and K32W148. AN14298 32kHz Cystal-Less Mode on KW45: This application note provides information on the 32 kHz Crystal-less mode on the KW45 device. This mode allows you to reduce the cost of the system, without compromising the 32 kHz clock accuracy.  AN13227 Hardware Design Considerations for KW45B41Z and K32W148 Bluetooth LE Devices: This application note describes printed-circuit board (PCB) design considerations for the KW45B41Z83AFTA, and KW45B41Z82AFTA and K32W1480VFTAT MKW35A, MKW36A, MKW35Z, and MKW36Z 40-pin HVQFN (6x6) and 48-pin Laminated QFN (HVLQFN-7x7 pitch 0.5 mm) wettable flank) package and KW45B41Z83AFPA and KW45B41Z82AFPA MKW35A, MKW36A, MKW35Z, and MKW36Z 40-pin HVQFN (6x6) and 40-pin Laminated QFN (HVLQFN-6x6 pitch 0.5 mm) wettable flank) package Power Management: AN13230: Kinetis KW45 and K32W1 Bluetooth LE Power Consumption Analysis This application note provides information about the power consumption of KW45 wireless MCUs, the hardware design and optimized for low power operation. AN13831: KW45/K32W1 Power Management Hardware This application note describes the usage of the different modules dedicated to power management in the KW45/K32W1 MCU. AN14664 Coin cell Hardware Recommendations for Kinetis Bluetooth LE Applications: This document describes some hardware and software solutions to minimize the peaks of current at the coin cell level RF: AN13687 : K32W1 Connectivity test for 802.15.4 Application This application note describes how to use the connectivity test tool to perform K32W1 802.15.4 RF performance. AN13728 : KW45 RF System Evaluation Report for Bluetooth LE and IEEE 802.15.4 Applications This application note provides the radio frequency evaluation test results of the KW45 board for BLE (2FSK modulation) and for IEEE 802.15.4 (OQPSK modulation) applications. Also describes the setup and tools that can be used to perform the tests.  AN14098: KW45-LOC RF Test Report This application note provides basic RF test result of the KW45B41Z localization board.  AN13228 : KW45-EVK RF System Evaluation Report for BLE Applications This application note provides the RF evaluation test result of the KW45B41Z-EVK for BLE application using two frequency Shift Keying modulation. AN13229 : KW45-EVK Co-existence with RF System Evaluation Report for BLE application This application note provides the RF evaluation test results of the KW45B41Z-EVK for BLE application (2FSK modulation) AN13512 : Kinetis Wireless Family Products BLE Coexistence with Wi-Fi Application This application note provides the K32W1/4X low energy family products immunity on Wi-Fi signals and methods to improve coexistence with Wi-Fi  AN14294 : Out of Band Implementation with KW45 This document explains the steps required to set up an Out of Band (OOB) pairing connection between two KW45 EVK boards, using UART and CAN communication interfaces to share OOB data. AN2731 Compact Planar Antennas for 2.5GHz Communication: This document is not an exhaustive inquiry into antenna design. It is instead focused on helping the customers understand enough board layout and antenna basics to select a correct antenna type for their application, as well as avoiding typical layout mistakes that cause performance issues that lead to delays AN14645 How to Use Random Static Device Address for Bluetooth Application: This document introduces how to enable Random Static Device Address for a Bluetooth Low Energy application. The default device address type in the SDK is Public Device Address. AN14112 Car Connectivity Consortium (CCC) Digital Key R3 - Bluetooth LE Vehicle Keyless Access System: This document provides a hardware and software platform to implement a simple CCC Digital Key Release 3.0 system. The hardware and software components of this system allow the user to get familiar with the CCC Digital Keys R3 specification and how it can be implemented using NXP products and tools. AN13953 Integrating NFC Reader Library in a KW4X Bluetooth Low Energy Application:  This document gives instructions on how to create a Bluetooth Low Energy (Bluetooth LE) project for the EVK-KW45 development board and MCUXpresso IDE, and how to integrate NFC Reader Library. AN13049 Wi-Fi/Bluetooth/802.15.4 M.2 Key E Pinout Definition: This document defines M.2 usage for both NXP Wi-Fi/Bluetooth and Tri-Radio M.2 module design Security: AN13859 : KW45/K32W1 In-System Programming Utility This application note provides steps to boot KW45/K32W1 MCU in ISP mode and establish various serial connections to communicate with the MCU. AN14003 : Programming the KW45 Flash for Application and Radio Firmware via Serial Wire Debug during mass production This application note describes the steps to write, burn and programming all the necessary settings via SWD in mass production.  AN13883 : Updating KW45 Radio Firmware Via ISP Using SPSDK This application note provides steps to boot KW45/K32W1 MCU in ISP mode and update the radio firmware with secure binary. AN14109 : KW45 and K32W148 Secure  Boot Using the SEC Tool This application note provides steps to do secure boot KW45/K32W1 MCU using signed images and secure binaries on the SEC GUI tool. AN13838 :  KW45 and K32W148 Secure  Boot Using the SPSDK Command line Tool This application note provides steps to do secure boot KW45/K32W1 MCU using signed images and secure binaries on the SPSDK command line tool. AN13931 : Managing Lifecycles on KW45 and K32W148 This application note provides steps to do transition lifecycles KW45/K32W1 MCU using the SEC GUI and SPSDK command line tools.  AN14158: Debug Authentication on KW45/ K32W148 This application note describes how to do debug authentication to securely debug an application in the field.  AN14544 : EdgeLock 2GO Services for MPU and MCU This application note introduces the EL2GO services for NXP devices. This allows trust provisioning of the device in an untrusted environment.  AN14174: KW45/K32W1 Flash Encryption using NPXThis application note provides steps to do enable on-the-fly encryption on KW45/K32W1 MCU. AN14158: debug authentication on KW45/K32W148 This application note describes the steps for debug authentication using the Secure Provisioning SDK tool (SPSDK). AN15038 EdgeLock 2GO Provisioning MCUs via Product Type using Secure Provisioning (SEC) Tool:  This document offers an outline of the EdgeLock 2GO platform and discusses the "Device provisioning via product type" flow. The document focuses on the initial device provisioning using secure objects from the EdgeLock 2GO cloud server. AN14670  EdgeLock 2GO Provisioning via SPSDK for MCUs: This document offers an outline of the EdgeLock 2GO platform and discusses the “Device provisioning via proxy” flow. The document focuses on the initial device provisioning using secure objects from the EdgeLock 2GO cloud server.  AN14624 EdgeLock 2GO Provisioning via Secure Provisioning Tool (SEC) for MCUs: This document offers an outline of the EdgeLock 2GO platform and discusses the "Device provisioning via proxy" flow. Useful Links [MCUXSDK] How to use GitHub SDK for KW4x, MCXW7x, MCXW2x - NXP Community this community post provides step by step how to use GitHub SDK [MCUXSDK] GitHub SDK - Documentation for Bluetooth LE platforms - NXP Community this community post provides the documentation for BLE platforms.  Clock Measuring using the Signal Frequency Analyzer (SFA) module for KW45/KW47/MCXW71/MCXW72 - NXP Community : this community provides the steps on how to use the Signal Frequency Analyzer  The best way to build a PCB first time right with KW45 (Automotive) or K32W1/MCXW71 (IoT/Industrial)... Community : In this community provides the important link to build a PCB using a KW45 or K32W148 and MCXW71 and all concerning the radio performances, low power and radio certification (CE/FCC/ICC) How to use the HCI_bb on Kinetis family products and get access to the DTM mode:  This article is presenting two parts: How to flash the HCI_bb binary into the Kinetis product. Perform RF measurement using the R&S CMW270 BLE HCI Application to set transmitter/receiver test commands: This article provides the steps to show how user could send serial commands to the device. Bluetooth LE HCI Black Box Quick Start Guide : This article describes a simple process for enabling the user controls the radio through serial commands. Kinetis (../45/47/43;MCX W71/72/70) & MCX W23 Power Profile Tools (including Localization):  This page is dedicated to the Kinetis (KW35/KW38/KW45/KW47/KW43) and MCX W7x (MCX W71/W72/W70) Power Profile Tools. It will help you to estimate the power consumption in your application (Automotive or IIoT) and evaluate the battery lifetime of your solution. KW45/K32W1 32MHz & 32kHz Oscillation margins: this article provides the properly configuration for the Oscillation margins for the circuit. KW45/MCXW71 Changing Clocking peripherals from FRO6M to other clock sources:  This article provides a comprehensive guide to selecting and configuring alternative clock sources   Reference Designs Bluetooth Ranging Access Vehicle Enablement System - NXP Community Blue Ravens (Bluetooth Ranging Access Vehicle Enablement System) is a system solution developed by NXP to assist customers in designing their own BLE-based car access solutions using NXP products. Demo (video) KW45 Based CS 1 to Many Demo NXP - Channel Sounding   Training BLE Introduction  RF Switch Comparison Absorptive/Reflective Standards Comparison ETSI / FCC / ARIB requirements BLE Channel Sounding  - Overview BLE Channel Sounding - RF Hardware BLE Channel Sounding - ANSYS Modeling Tools  BLE Channel Sounding - Antenna Prototypes Validation Measurements     Equipment Wireless Equipment: This article provides the links to the Equipment that helps to the project development  Development Tools  SDK builder: The MCUXpresso SDK brings open-source drivers, middleware, and reference example application to speed your software development. SDK GitHub: SDK open-source Drivers, middleware and reference examples in Github NXP MCUXpresso: MCUXpresso IDE offers advanced editing, compiling and debugging features with the addition of MCU-Specific debugging. Supports connections with all general-purpose Arm Cortex-M.  NXP SPSDK: Is a unified, reliable, and easy to use Python SDK library working across the NXP MCU portfolio providing a strong foundation from quick customer prototyping up to production deployment. NXP SEC Tool: The MCUXpresso Secure Provisioning Tool us a GUI-based application provided to simplify generation and provisioning of bootable executables on NCP MCU devices. NXP OTAP Tool: Is an application that helps the user to perform an over the air firmware update of an NXP development board. Config Tool: MCUXpresso Config Tools, an integrated suite of configuration tools, these configuration tools allow developers to quickly build a custom SDK and leverage pins, clocks and peripheral to generate initialization C code or register values for custom board support. SDK Examples for Wireless MCUs: The wireless examples feature many common Bluetooth configurations. **For secure files is necessary to request additional access.  KW45
記事全体を表示
KW45 知识中心 KW45 的三核架构集成了一个 96 MHz CM33 应用核心、专用 CM3 无线模块内核和一个隔离的 EdgeLock 安全区域。基于闪存的无线模块内核具有专用 SRAM,可提供高度可配置和可升级的软件实施无线模块,从而将主内核上的资源释放给客户应用空间。 符合低功耗蓝牙 5.3 标准的无线模块最多可同时支持 24 个安全连接。EdgeLock 安全区域的隔离执行环境提供了一套加密加速器、密钥存储操作和安全生命周期管理,最大限度地减少了主要内核安全责任。 KW45 MCU 还集成了 FlexCAN,有助于无缝集成到汽车的车载或工业 CAN 通信网络中。FlexCAN 模块可以支持 CAN 的灵活数据传输速率 (CAN FD),以实现更高带宽和更低延迟。 KW45 方框图 KW45 架构框图 文件 参考手册 Datasheet Errata Secure Reference 手册** 认证 SESIP 认证 SESIP ST PSA认证 RED 认证 欧盟符合性声明 (EVK) 欧盟符合性声明(LOC) 日本 MIC KW45-LOC _TELEC-20250221请参见下方附件 蓝牙规范 蓝牙 5.0 功能概述 蓝牙 5.1 功能概述 蓝牙 5.2 功能概述 Bluetooth_5.3_功能概述 Bluetooth_5.4_功能概述 Bluetooth_6_Feature_Overview 评估板 KW45 KW45-EVK KW45-EVK 原理图 KW45-EVK设计文件 KW45-EVK 用户手册 KW45-LOC 用户手册 KW45-EVK快速入门 应用笔记 软件、硬件和外设: AN14122 :如何在 KW45 上使用 RTC本应用笔记介绍了如何在 BLE 演示中配置和使用 RTC 外围设备 AN14141:在 KW45 低功耗蓝牙连接堆栈中启用看门狗定时器模块 。本应用笔记描述了在连接堆栈演示中实现 WDOG 定时器的过程。 AN13855:将 OTAP 客户端服务集成到 KW45/K32W1 蓝牙 LE 外围设备中 本应用笔记提供了将空中编程客户端服务集成到 BLE 外围设备的步骤和过程。 AN13584:Kinetis KW45 和 K32W1 负载拉动报告 本应用笔记描述了负载拉动特性的测量方法及相关结果。 AN13860:使用 OTAP 工具为 KW45/K32W1 创建固件更新镜像 本应用笔记提供了通过 OTAP 工具在 KW45 开发板上创建并升级镜像的步骤。 AN14077:将 KW45 (1MB) 迁移至 KW45 (512kB) 的步骤  本应用笔记描述了从 1MB 闪存迁移至 512kB 闪存所需的初始步骤。 电源管理: AN13230:Kinetis KW45 和 K32W1 蓝牙低功耗 (BLE) 功耗分析  本应用笔记提供了关于 KW45 无线微控制器 (MCU) 的功耗信息,包括硬件设计及优化以实现低功耗运行。 AN13831:KW45/K32W1 电源管理硬件  本应用笔记描述了在 KW45/K32W1 微控制器中用于电源管理的不同模块的使用方法。 射频: AN13687:K32W1 802.15.4 应用连接性测试 本应用笔记介绍了如何使用连接性测试工具来测试 K32W1 802.15.4 的射频性能。 AN13728:KW45 射频系统评估报告(适用于蓝牙低功耗和 IEEE 802.15.4 应用)本应用笔记提供了 KW45 开发板在蓝牙低功耗(2FSK 调制)和 IEEE 802.15.4(OQPSK 调制)应用中的射频评估测试结果。还描述了可以用于执行测试的设置和工具。  AN14098: KW45-LOC 射频测试报告  本应用笔记提供了KW45B41Z定位板的基本射频测试结果。  AN13228:用于 BLE 应用的 KW45-EVK 射频系统评估报告 本应用笔记提供了 KW45B41Z-EVK 在 BLE 应用中使用二进制频移键控调制的射频评估测试结果。 AN13229:KW45-EVK 与射频系统共存的评估报告(适用于 BLE 应用)本应用笔记提供了 KW45B41Z-EVK 在 BLE 应用(2FSK 调制)中的射频评估测试结果 AN13512:Kinetis 无线产品系列 BLE 与 Wi-Fi 共存应用  本应用笔记介绍了 K32W1/4X 低功耗产品系列对 Wi-Fi 信号的抗干扰能力,并提供了改善与 Wi-Fi 共存的方法  安全性: AN13859:KW45/K32W1 系统内编程工具  本应用笔记提供了在 ISP 模式下启动 KW45/K32W1 微控制器并建立各种串行连接以与微控制器通信的步骤。 AN1403:在批量生产中通过串行线调试(SWD)为KW45闪存编程以应用和无线固件 。本应用笔记详细介绍了在批量生产中通过SWD编写、烧录和设置所有必要参数的步骤。  AN13883: 通过 SPSDK 使用 ISP 更新 KW45 无线电固件  本应用笔记提供了在 ISP 模式下启动 KW45/K32W1 MCU 并使用安全二进制文件更新无线电固件的步骤。 AN14109:使用SEC工具实现KW45和K32W148安全启动 本应用笔记提供了使用 SEC GUI 工具,通过签名镜像和安全二进制文件实现 KW45/K32W1 MCU 安全启动的步骤。 AN13838:KW45 和 K32W148 安全启动使用 SPSDK 命令行工具本应用笔记提供了使用 SPSDK 命令行工具,通过签名镜像和安全二进制文件实现 KW45/K32W1 MCU 安全启动的步骤。 AN13931:KW45 和 K32W148 的生命周期管理 本应用笔记提供了使用 SEC GUI 和 SPSDK 命令行工具来转换 KW45/K32W1 MCU 的过渡生命周期的步骤。 AN14174:KW45/K32W148 使用 NPX 进行闪存加密本应用笔记提供了在 KW45/K32W1 微控制器上启用实时加密的步骤。 AN14158:KW45/K32W148 上的调试认证本应用笔记介绍了如何进行调试认证,以便在现场安全地调试应用程序。  AN14544:EdgeLock 2GO 服务适用于 MPU 和 MCU 本应用笔记介绍了 NXP 设备的 EL2GO 服务。该服务允许在不受信任的环境中为设备进行信任配置。 支持 如果您对 KW45 有任何疑问,请在我们的无线 MCU 社区中留下您的问题!此处 有用链接 参考设计 - NXP 社区 [MCUXSDK] 如何使用 GitHub SDK 适用于 KW4x、MCXW7x、MCXW2x - NXP 社区此社区帖子逐步介绍了如何使用 GitHub SDK [MCUXSDK] GitHub SDK - 蓝牙 LE 平台文档 - NXP 社区此社区帖子提供了 BLE 平台的文档。  使用 KW45/KW47/MCXW71/MCXW72 的信号频率分析仪 (SFA) 模块进行时钟测量 - NXP 社区:该社区提供了如何使用信号频率分析仪的步骤 首次正确构建 PCB 的最佳方式是使用 KW45(汽车)或 K32W1/MCXW71(物联网/工业)... 社区:在此社区中,您可以找到使用 KW45 或 K32W148 和 MCXW71 构建 PCB 的重要链接,所有链接均涉及无线电性能、低功耗和无线电认证 (CE/FCC/ICC) 如何在 Kinetis 系列产品上使用 HCI_bb 并进入 DTM 模式:本文分为两部分: 如何将HCI_bb二进制文件烧录到Kinetis产品中。 使用 R&S CMW270 进行射频测量 BLE HCI 应用程序设置发射机/接收机测试命令:本文提供了相关步骤,展示用户如何向设备发送串行命令。 Bluetooth LE HCI 黑盒快速入门指南:本文介绍了一个简单流程,能让用户通过串行命令控制无线电。 Kinetis (K32/38/KW45 & K32W1/MCXW71)功率配置工具: 此页面专门介绍 Kinetis (KW35/KW38/KW45) 和 MCX W7x (MCX W71) 功率配置工具。它将帮助您估算您的应用程序(汽车或物联网)的功耗,并评估您解决方案的电池寿命。 KW45/K32W1 32MHz 和 32kHz 振荡裕度:本文提供了电路中振荡裕度的正确配置。 基于 KW45 的 CS 1 对多演示NXP - 信道探测   培训 BLE Introduction  射频开关比较 吸收型/反射型 ETSI / FCC / ARIB 标准比较与要求 BLE 信道探测  - 概述 BLE 信道探测 - RF 硬件 BLE 信道探测 - ANSYS 建模工具 BLE 信道探测 - 天线原型验证测量 设备 无线设备: 本文提供了有助于项目开发的设备链接  开发工具  SDK 构建器: MCUXpresso SDK 提供开源驱动程序、中间件和参考示例应用程序,以加快软件开发。 SDK GitHub:SDK 开源驱动程序、中间件和参考示例在 GitHub 上。 NXP MCUXpresso: MCUXpresso 集成开发环境 (IDE) 提供了高级编辑、编译和调试功能,并增加了 MCU 专用的调试功能。支持与所有通用 Arm Cortex-M 的连接。  NXP SPSDK:是一个统一、可靠且易于使用的Python SDK库,适用于 NXP MCU 产品组合,为客户快速制作原型到生产部署提供坚实的基础。 NXP SEC工具: MCUXpresso安全配置工具是一款基于 GUI 的应用程序,用于简化在 NCP MCU 设备上生成和配置可启动的可执行文件。 NXP OTAP Tool: 是一款帮助用户对 NXP 开发板执行空中固件更新的应用程序。 配置工具: MCUXpresso 配置工具是一套集成的配置工具套件,这些工具允许开发人员快速构建自定义 SDK,并利用引脚、时钟和外设生成初始化 C 代码或自定义板支持的寄存器值。 无线 MCU 的 SDK 示例: 这些无线示例包含许多常见的蓝牙配置。 **对于安全文件,必须请求额外的访问权限。  动手实践培训 产品:K32W1 协议:802.15.4 协议:BLE -> 连接性 协议:蓝牙 协议:Matter 协议:Thread 协议:Zigbee
記事全体を表示
FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC Dear All In the download page https://www.nxp.com/design/design-center/software/development-software/freemaster-run-time-debugging-tool:FREEMASTER There is the package pberna67_1-1790030347425.png However if you click the Download button, no download stats.  I need to support LPC1766, but it seams it is not supported by version 3 (strange because the Driver is indicated), but still I don't see any driver in version V2 for LPC1766 Thanks Paolo Re: FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC Dear Michael Thanks for your fast replay! I'm already using Jlink/MCU Link and MCU Link2 without any driver, to read/write variables, however I would like to add also the Application Command management (nothing more than that). I don't need any support of USB/UART/CAN ect... interface support. " The "dreg" directory then contains drivers which do not depend on the SDK at all. The "dreg" drivers use a direct register access instead - this is basically what you need, but unfortunately again, the legacy LPC is not in the list." With this additional limitations, do you think that  dreg directory contents  is enough  for me ? I read  that V2 version the driver should support also LPC1766. Is it true ? Can you send me this driver? Thanks Paolo Re: FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC Dear Paolo, the link you used to get the FreeMASTER driver is correct.  Unfortunately, this driver only supports the newer devices supported by NXP MCUXpresso SDK. The LPC1766 is not supported by the SDK. There are two options for you when using LPC1766: - Use FreeMASTER over JTAG (Segger J-Link or LPCLink2/CMSIS-DAP) - This will enable you to inspect and control variables. No communication driver is needed, FreeMASTER accesses the memory while the MCU is running. - Get the driver for a different part and port it to LPC1766. See more details below: The reason for the SDK dependency is that the FreeMASTER driver layers its communication drivers on top of SDK low-level drivers. You can still get the full FreeMASTER "middleware" driver from the SDK builder link when you select one of supported MCUs, such as (e.g. MCXN947). After downloading you will find the FreeMASTER code in the middleware/freemaster directory. Note that there are also other drivers in the FreeMASTER package (in the src/drivers), that might be partially useful to you. The mcuxsdk directory contains the primary drivers based on SDK low-level - you can still look at them to understand how the FreeMASTER driver code is structured. The "dreg" directory then contains drivers which do not depend on the SDK at all. The "dreg" drivers use a direct register access instead - this is basically what you need, but unfortunately again, the legacy LPC is not in the list. We have this kind of drivers for NXP DSC, Kinetis, Power Architecture, S12Z and S32 platforms. Porting this concept to LPC shall be quite straightforward task. Regards, Michal Re: FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC Dear Michael, You convinced me to use the direct JLink SWD connection without the support of your Application Command (so there is no need to port the driver to the LPC1766). However, I just discovered that I also need to support the TSA table. In fact, I want to build a configurator for my product (parameter read/write), but it can happen that the firmware in it changes version. I don't have any display to know that version number, so it is not possible to know in advance which firmware image version is loaded, which means it is not possible to load the right .AXF file in FreeMaster in advance. I need to read the address of the variables from the host processor, so unfortunately I need to port the target driver :(, unless there are other ways to work around this problem. The only doubt I have is that you wrote: "You can see that this simple function operates directly on UART peripheral registers. Porting this to LPC means creating similar functions which operate on the LPC UART module (which is different from the Kinetis one)." I shouldn't need to port any peripheral communication driver (UART, CAN, USB), because I only need to support SWD. Is that correct? Can you elaborate more the porting "path trace" for only this option? Paolo Re: FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC Hello Paolo, no, the V2 driver does not support the LPC. It supports some legacy platforms such as HCS08, HCS12, ColdFire or PowerPC, but not the LPC. If your motivation is just to enable Application Commands, I would suggest that it would be much easier and generally a better solution to change the way how your application is controlled. Application Commands can be easily replaced by picking a few variables into which FreeMASTER writes the control request parameters and use another variable as a "request to process". Once the target application discovers this request variable set, it can process the control command and acknowledge it by resetting the request variable back to zero. This behavior is functionally equal to Application Commands, and it enables to operate over JTAG without any communication driver. To answer your other question: The "dreg" drivers are not directly usable for you. As I wrote, the LPC is not supported, but you can create the port quite easily yourself. If you look at one of UART files such as freemaster_kxx_uart.c, you can find driver functions making atomic UART operations. For example enabling interrupts: You can see, that this simple function operates directly on UART peripheral registers. Porting this to LPC means creating similar functions which operate on LPC UART module (which is different from Kinetis one). Regards, Michal Re: FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC Dear Michael I made the porting of the freemaster_examples/fmstr_example_pdbdm of the lpcxpresso54114 SDK in  the LPC1768 platform using the Keil MCB1700 board . Everything work well. NXP did a very good job, no change in code during the porting activity, it is a very simple task Unfortunately is not possible to attach it the to this forum as .zip file Regards Paolo Thanks and regards
記事全体を表示
FreeMASTER 通信驱动程序 3.0,适用于 i.MX、LPC、Kinetis 和 DSC 各位 在下载页面 https://www.nxp.com/design/design-center/software/development-software/freemaster-run-time-debugging-tool:FREEMASTER 包裹在这里。 pberna67_1-1790030347425.png 但是,如果您点击“下载”按钮,则不会显示下载统计数据。我需要支持 LPC1766,但版本 3 似乎不支持(很奇怪,因为驱动程序明明已经标明了),而且我在版本 2 中仍然找不到 LPC1766 的驱动程序。 谢谢 Paolo Re: FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC 亲爱的迈克尔 感谢您的快速回复! 我目前已经在使用 Jlink/MCU Link 和 MCU Link2,无需任何驱动程序即可读取/写入变量,但我还想添加应用程序命令管理功能(仅此而已)。我不需要任何USB/UART/CAN等接口支持。 “dreg”目录则包含完全不依赖于SDK的驱动程序。“dreg”驱动程序改用直接寄存器访问——这基本上就是你需要的,但不幸的是,传统的LPC不在列表中。 考虑到这些额外的限制,您认为 dreg 目录的内容对我来说足够了吗? 我看到有资料说V2版本的驱动程序也应该支持LPC1766。这是真的吗?你能把这个驱动程序发给我吗? 谢谢保罗 Re: FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC 亲爱的保罗, 您用来获取FreeMASTER驱动程序的链接是正确的。遗憾的是,该驱动程序仅支持 NXP MCUXpresso SDK 支持的较新设备。SDK 不支持 LPC1766。 使用 LPC1766 时,您有两种选择: - 通过 JTAG(Segger J-Link 或 LPCLink2/CMSIS-DAP)使用 FreeMASTER - 这将使您能够检查和控制变量。无需通信驱动程序,FreeMASTER 可在 MCU 运行时访问内存。 - 获取其他部件的驱动程序并将其移植到 LPC1766。更多详情请见下文: 之所以存在 SDK 依赖关系,是因为 FreeMASTER 驱动程序将其通信驱动程序构建在 SDK 底层驱动程序之上。当您选择支持的 MCU 之一时,例如(例如),您仍然可以从 SDK 构建器链接获取完整的 FreeMASTER“中间件”驱动程序。MCXN947)。下载完成后,您将在 中间件/freemaster 目录中找到 FreeMASTER 代码。 请注意,FreeMASTER 软件包(位于 src/drivers 中)中还有其他驱动程序,这些驱动程序可能对您部分有用。mcuxsdk 目录包含基于 SDK 底层的主要驱动程序 - 您仍然可以查看它们以了解 FreeMASTER 驱动程序代码的结构。“dreg”目录则包含完全不依赖于SDK的驱动程序。“dreg”驱动程序使用直接寄存器访问——这基本上就是你需要的,但不幸的是,传统的LPC不在列表中。我们有适用于 NXP DSC、Kinetis、Power Architecture、S12Z 和 S32 平台的此类驱动程序。将这个概念移植到LPC应该是一项相当简单的任务。 问候, 米哈尔 Re: FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC 亲爱的迈克尔: 你说服我使用直接的 JLink SWD 连接,而不需要你的应用程序命令的支持(因此无需将驱动程序移植到 LPC1766)。然而,我刚刚发现我还需要支持 TSA 表格。事实上,我想为我的产品构建一个配置器(参数读取/写入),但其中的固件版本可能会发生变化。我没有显示版本号,因此无法预先知道加载的是哪个固件映像版本,这意味着无法预先在 FreeMaster 中加载正确的 .AXF 文件。我需要从主机处理器读取变量的地址,所以很遗憾,我需要移植目标驱动程序 :(,除非有其他方法可以解决这个问题。 我唯一的疑问是,你写道: “可以看到,这个简单的函数直接操作 UART 外设寄存器。将此移植到 LPC 意味着创建类似的功能,这些功能在 LPC UART 模块上运行(该模块与 Kinetis 的 UART 模块不同)。 我不需要移植任何外围通信驱动程序(UART、CAN、USB),因为我只需要支持 SWD。是这样吗?能否详细说明一下仅针对此选项的移植“路径跟踪”? 保罗 Re: FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC 你好,保罗, 不,V2驱动程序不支持LPC。它支持一些旧平台,如 HCS08、HCS12、ColdFire 或 PowerPC,但不支持 LPC。 如果你的动机仅仅是启用应用程序命令,我建议改变应用程序的控制方式会更容易,通常也是更好的解决方案。可以通过选择几个变量来轻松替换应用程序命令,FreeMASTER 会将控制请求参数写入这些变量,并使用另一个变量作为“要处理的请求”。一旦目标应用程序发现此请求变量集,它就可以处理控制命令,并通过将请求变量重置为零来确认该命令。这种行为在功能上等同于应用程序命令,它允许在没有任何通信驱动程序的情况下通过 JTAG 进行操作。 关于你的另一个问题:你无法直接使用“dreg”驱动程序。正如我之前所说,LPC 不受支持,但您可以很轻松地自己创建端口。如果你查看像 freemaster_kxx_uart.c 这样的 UART 文件,你会发现驱动程序函数可以执行原子 UART 操作。例如,启用中断: 您可以看到,这个简单的函数直接操作 UART 外设寄存器。将其移植到 LPC 意味着创建在 LPC UART 模块(与 Kinetis UART 模块不同)上运行的类似功能。 问候, 米哈尔 Re: FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC 亲爱的迈克尔 我使用 Keil MCB1700 板将 lpcxpresso54114 SDK 的 freemaster_examples/fmstr_example_pdbdm 移植到了 LPC1768 平台上。一切运转良好。NXP做得非常好,移植过程中代码没有做任何改动,这是一项非常简单的任务。 很遗憾,无法将其以 .zip 格式附加到此论坛。文件 问候 保罗 谢谢,此致敬礼。
記事全体を表示
FreeMASTER Communication Driver 3.0 for i.MX、LPC、Kinetis、DSC 親愛なるみんな ダウンロードページで https://www.nxp.com/design/design-center/software/development-software/freemaster-run-time-debugging-tool:FREEMASTER パッケージが pberna67_1-1790030347425.png しかし、ダウンロードボタンをクリックしても、ダウンロード統計は表示されません。LPC1766をサポートする必要がありますが、バージョン3ではサポートされていないようです(ドライバが示されているのに不思議です)。それでもバージョンV2にはドライバが見当たりませんLPC1766 ありがとうございます パオロ Re: FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC 親愛なるパオロ、 FreeMASTERドライバーを入手するために使ったリンクは正しいです。残念ながら、このドライバーはNXP MCUXpresso SDKでサポートされる新しいデバイスのみに対応しています。このLPC1766はSDKでサポートされていません。 LPC1766を使用する際には、以下の2つの選択肢があります。 - JTAG (Segger J-Link または LPCLink2/CMSIS-DAP) を介して FreeMASTER を使用する - これにより、変数を検査および制御できるようになります。通信ドライバは不要で、FreeMASTERはMCUが稼働中もメモリにアクセスします。 - ドライバーを別の部品に取り寄せて、LPC1766に移植する。詳細は下記をご覧ください。 SDK依存の理由は、FreeMASTERドライバーが通信ドライバーをSDKの低レベルドライバーの上に重ねているからです。サポートするMCUのいずれかを選択すると、SDKビルダーリンクからFreeMASTERのフル「ミドルウェア」ドライバーを入手できます。例えば(例:MCXN947)。ダウンロード後、FreeMASTERのコードはmiddleware/freemasterディレクトリにあります。 FreeMASTERパッケージ(src/drivers)には他にも、あなたにとって役立つ可能性のある他のドライバーも含まれます。mcuxsdkディレクトリにはSDKの低レベルに基づくプライマリドライバーが入っていますが、FreeMASTERのドライバーコードの構造を理解するためにも確認できます。「dreg」ディレクトリにはSDKに依存しないドライバーが含まれています。「デレッグ」ドライバは代わりにダイレクトレジスタアクセスを使っています。これは基本的に必要なものですが、残念ながらレガシーLPCはリストに含まれていません。NXP DSC、Kinetis、Power Architecture、S12Z、S32プラットフォーム向けのこのようなドライバーがあります。この概念をLPCに移植するのは非常に簡単な作業となるだろう。 よろしくお願いいたします。 ミハル Re: FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC マイケル様 迅速なご返信ありがとうございます! 私はすでにJlink/MCU LinkとMCU Link2をドライバーなしで使って変数の読み書きに使っていますが、アプリケーションコマンドマネジメント(それ以上のものではありません)も追加したいと思っています。USB/UART/CAN などのサポートは必要ありません...インターフェースのサポートです。 「dreg」ディレクトリにはSDKに依存しないドライバーが含まれています。「デレッグ」ドライバは代わりにダイレクトレジスタアクセスを使っています。これは基本的に必要なものですが、残念ながらレガシーLPCはリストに含まれていません。」 これらの追加制限を踏まえて、dregディレクトリの内容だけで十分だと思いますか? V2バージョンのドライバーもLPC1766対応していると読みました。それは本当ですか?このドライバーを送ってもらえますか? ありがとう、パオロ。 Re: FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC こんにちは、パオロさん。 いいえ、V2ドライバーはLPCをサポートしていません。HCS08、HCS12、ColdFire、PowerPCなどの一部のレガシーなプラットフォームをサポートしていますが、LPCはサポートしていません。 もし単にアプリケーションコマンドを有効にしたいだけなら、アプリケーションの制御方法を変える方がずっと簡単で一般的により良い解決策だと思います。アプリケーションコマンドは、FreeMASTERが制御リクエストパラメータを書き込む変数をいくつか選び、別の変数を「処理リクエスト」として使うことで簡単に置き換えられます。ターゲットアプリケーションがこのリクエスト変数セットを検出すると、制御コマンドを処理し、リクエスト変数をゼロに戻して確認できます。この動作は機能的にアプリケーションコマンドと同等であり、通信ドライバなしでJTAG上で動作することを可能にします。 もう一つの質問に答えると、「ドレッグ」ドライバは直接使えるものではありません。前述の通り、LPCはサポートされていませんが、自分で簡単にポートを作成できます。freemaster_kxx_uart.cのようなUARTファイルを見ると、原子的なUART操作を行うドライバ関数が見つかります。例えば、割り込みを有効にする場合: この単純な関数はUART周辺レジスタ上で直接動作していることがわかります。これをLPCに移植するには、LPC UARTモジュール(Kinetis Oneとは異なる)上で動作する類似の関数を作成する必要があります。 よろしくお願いいたします。 ミハル Re: FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC 親愛なるマイケルへ、 あなたのために、Application Commandのサポートなしで直接JLink SWD接続を使うよう説得されました(つまり、ドライバーをLPC1766に移植する必要はありません)。しかし、最近気づいたのはTSAテーブルもサポートしなければならないということです。実は、自分の製品用にコンフィギュレーター(パラメータ読み書き)を作りたいのですが、その中のファームウェアがバージョンを変えてしまうことがあります。バージョン番号を知るためのディスプレイがないため、事前にどのファームウェアイメージバージョンが読み込まれているかを知ることはできず、正しいFreeMasterのAXFファイルを事前に読み込むことはできません。ホストプロセッサから変数のアドレスを読み取る必要があるので、残念ながらターゲットドライバーを:(に移植する必要があります。他にこの問題を回避する方法がない限り。 唯一の疑問は、あなたがこう書いていることです: 「この単純な関数がUARTペリフェラルレジスタに直接動作していることがわかります。これをLPCに移植するには、LPC UARTモジュール(Kinetisとは異なる)上で動作する類似の機能を作る必要があります。」 ペリフェラル通信ドライバ(UART、CAN、USB)を移植する必要はないはずです。なぜならSWDをサポートすれば十分だからです。それは正しいですか?このオプションだけの「パストレース」について、もう少し詳しく教えてもらえますか? パオロ Re: FreeMASTER Communication Driver 3.0 for i.MX, LPC, Kinetis and DSC 親愛なるマイケルへ 私は Keil MCB1700 ボードを使って、lpcxpresso54114 SDK のfreemaster_examples/fmstr_example_pdbdmをLPC1768プラットフォームに移植しました。すべて順調に動作しています。NXPは非常に良い仕事をした。移植作業中にコードの変更は一切なく、非常に簡単な作業だった。 残念ながら、このフォーラムに.zipファイルとして添付することはできません。ファイル よろしくお願いいたします パオロ ありがとうございます。
記事全体を表示
促销优惠券 您好, 为什么我的促销优惠券“ADCWFBXT”对FRDM-MCXN236无效? 普拉莫德·乔格卡 [email protected] 开发板 FRDM 培训 Re: PROMO Coupon 连我都无法使用FRDM-MCXN236 的促销优惠券。 Re: PROMO Coupon 请注意,优惠券 ADCWFBXT 的有效期至 2025 年 12 月 30 日。正如我们网站上所说: FRDM 创新——由我们负责!   祝您今天愉快。 Re: PROMO Coupon FRDM-MCXN236主板还有其他优惠券吗?
記事全体を表示
FRDM-MCXN236にはクーポンは適用されません NXPのウェブサイトでは、この無料ボードを使って始められると宣伝していた。しかし、在庫があるにもかかわらず、クーポンコードがチェックアウト時にまだ使えません。 評価ボード Re: Coupon not valid for FRDM-MCXN236 こんにちは、 PLACEHOLDER7 その場合は、 [email protected] までにショッピングカートチームまでメールをお送りください。 そのチームはオンライン注文を担当しています。 ご理解いただきありがとうございます。 ベッキー
記事全体を表示
LS1046A カスタムデザインHRESET_Bリリースされていません <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、 LS1046Aプロセッサーを活用したカスタムデザインを作ろうとしています。(基板設計ではRDBを基準にしていました。)すべての電源レール電圧が正しいことを確認し、電源シーケンスのタイミングを測定したところ、すべてデータシートに記載されている許容範囲内であることが確認されました。私が経験している問題は、プロセッサーをリセットから解除できないことです。測定したところ、プロセッサーがHRESET_B信号を放っていません。リファレンスマニュアルによると、初期化中はプロセッサがこのラインを低く保ち、RCWの読み込みやPLLのロック後はリリースするそうです。RCWにエラーがあるのかと思い、代わりに内蔵のRCW値を使いました。(プロセッサに0x9Eと0x9F RCWの両方を固定しましたが、結果は同じでした。) 今のところ、私は少し途方に暮れています。クロックは納期通りに納品され、スルーレートはすべて仕様範囲内であり、ストラップ値を解放する前に適切な時間保持しています。リファレンスマニュアルには、PBLがエラーに遭遇した場合にRESET_REQ信号を切り替えると書かれていますが、私はそのような現象は見ていません。私の現時点での結論は、PBLが実行されていないということです。これはプロセッサがまだリセット状態にあるサインです。 何か見落としている点があるのでしょうか?次にどこを探せばいいでしょうか?私のタイミングは仕様の範囲内ですが、RDBとは完全に一致しません(ボード上の関連信号をプローブしました)。LS1046の電源シーケンス制御はどの程度敏感ですか? よろしくお願いいたします。 Re: LS1046A Custom Design HRESET_B not released こんにちは、ブライス 正しい方向にするためにどのシーケンスを変更したのか説明してもらえますか?現在、私もカスタムLS1046Aボードで同様の問題に直面しています。 Re: LS1046A Custom Design HRESET_B not released <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 上記のご回答、ありがとうございました。 最後に、CPLDコードのパワーシーケンスの問題を解決しました。元のコードがこの問題を引き起こしていたため、コードを書き直したところ、問題は解消されました。 Re: LS1046A Custom Design HRESET_B not released <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> プロセッサ接続の回路図を確認できるように、技術CASEを作成してください。 Re: LS1046A Custom Design HRESET_B not released <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> ハードウェアには、フラッシュメモリから取得したRCWではなく、ハードコードされたRCWを使用するように設定しました。 Re: LS1046A Custom Design HRESET_B not released <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> RCWが外部フラッシュメモリから読み取られているかどうかを、デジタルオシロスコープを使用して確認してください。 Re: LS1046A Custom Design HRESET_B not released <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> こんにちは、 ご回答ありがとうございます。上記すべてが良好な状態であることを確認しました。ただし、最後の点について一つ質問があります。これは電源投入リセットシーケンスを完了するために必要な手順なのでしょうか?先ほど述べたように、RESET_REQ信号を観測できないため、PBLの実行はできないと考えています。SerDesリファレンスクロックは、PBLを実行するために必須ですか、それともPBLがシステムをセットアップしている段階で必要になりますか? よろしくお願いします。 Re: LS1046A Custom Design HRESET_B not released <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 最初の確認段階として、以下を点検してください。 1) QorIQ LS1046A、LS1026Aデータシートの表1の注記に明示的に記載されているすべての信号のPORレベル。バスごとのピン配置リスト。 2) HRESET_Bは外部からアサートされない 3) SerDesリファレンスクロックはデータシートの要件に準拠しています。 問題が解決しない場合は、次のブリングアップステージを技術ケースとして行う方が便利です。 https://community.nxp.com/thread/381898
記事全体を表示
LS1046A Custom Design HRESET_B not released Hello, I am working to bringup a custom design making use of the LS1046A processor. (Board design used the RDB as a reference).  I have verified that all power rail voltages are correct and have have measured the power sequencing timing which all appear to be withing the tolerances found in the datasheet. The issue I am experiencing is that I am not able to bring the processor out of reset. When measuring, I found that the processor is not releasing the HRESET_B signal. The reference manual indicates that the processor will hold this line low while it is performing initialization and will release it after loading the RCW and locking PLL's, etc. Thinking perhaps I had an error in my RCW, I used the built-in RCW values instead. (I strapped the processor with both the 0x9E and 0x9F RCW values with the same result). At this point, I'm at a bit of a loss. My clocks are provided on time, my slew rates are all within spec, and I am holding the strapping values for the correct amount of time before releasing them. The reference manual also indicates that the PBL will toggle the RESET_REQ signal if it has encountered an error, but I am not seeing this happen. So my conclusion currently is that the PBL is not even being executed which, to me, is a sign that the processor is still in a reset state. Is there something here that I am missing? Anywhere I should look next? My timings are within spec, but do not match the RDB exactly (I probed the relevant signals on the board). How sensitive is the power sequencing on the LS1046? Thanks in advance. Re: LS1046A Custom Design HRESET_B not released Hi bryce  Can you explain what sequence did you chnage to get it right? Currently I am also facing similar issue with cutsom ls1046a board Re: LS1046A Custom Design HRESET_B not released Thank you for your above answers. To tie off the thread, I have solved the issue with the power sequencing in my CPLD code. Because the original code I had was causing this issue, I re-wrote it and I no longer see the issue.  Re: LS1046A Custom Design HRESET_B not released Please create a Technical Case so I will be able to check the processor connection schematics. Re: LS1046A Custom Design HRESET_B not released We have strapped the hardware to use the hard-coded RCW, not the RCW from flash. Re: LS1046A Custom Design HRESET_B not released Please use a digital scope to check whether RCW is read from an external flash. Re: LS1046A Custom Design HRESET_B not released Hello, Thanks for your response.  I have verified that all of the above are in a good state. One question I did have about your last point, however: Is this required in order for the power-on reset sequence to complete? As I stated earlier, we are not able to observe the RESET_REQ signal, so I believe we are unable to execute the PBL. Are SerDes reference clocks required in order execute the PBL, or are they required later on while PBL is already setting up the system? Thanks Re: LS1046A Custom Design HRESET_B not released As first checking stage please inspect: 1) POR levels of all signals explicitly mentioned in the notes to the QorIQ LS1046A, LS1026A Data Sheet, Table 1. Pinout list by bus. 2) HRESET_B is not asserted externally 3) SerDes reference clocks conform to the Data Sheet requirements. If the issue will not be resolved, it is more convenient to perform next bring-up stage as Technical Case: https://community.nxp.com/thread/381898 
記事全体を表示
此优惠券不适用于 FRDM-MCXN236 NXP 网站宣传了这款免费板。但是即使商品有库存,结账时优惠券代码仍然无法使用。 评估板 Re: Coupon not valid for FRDM-MCXN236 你好PLACEHOLDER7 在这种情况下,请您发送电子邮件至[email protected]联系我们的购物车团队。 该团队负责处理线上订单。 谢谢您的理解 贝基
記事全体を表示
LS1046A 定制设计 HRESET_B 未发布 <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好, 我正在努力开发一个使用 LS1046A 处理器的定制设计。(电路板设计参考了RDB。)我已经确认所有电源轨电压均正确,并且测量了电源时序时序,所有参数似乎都在数据手册规定的容差范围内。我遇到的问题是无法将处理器从重置状态中恢复。测量时,我发现处理器没有释放 HRESET_B 信号。参考手册指出,处理器在执行初始化时会将此线路保持低电平,并在加载 RCW 和锁定 PLL 等操作后将其释放。考虑到我的 RCW 设置可能有误,我改用了内置的 RCW 值。(我分别用 0x9E 和 0x9F RCW 值给处理器加装了 RCW 参数,结果相同)。 此时此刻,我有点不知所措。我的时钟按时交付,我的转换速率均在规格范围内,并且在释放之前,我会将捆扎值保持正确的时间。参考手册还指出,如果 PBL 遇到错误,它会切换 RESET_REQ 信号,但我没有看到这种情况发生。因此,我目前的结论是 PBL 根本没有执行,在我看来,这表明处理器仍处于 RESET 状态。 我是不是漏掉了什么?接下来我应该从哪里入手?我的时序符合规格,但与 RDB 不完全匹配(我探测了板上的相关信号)。LS1046的电源时序控制有多敏感? 先行致谢。 Re: LS1046A Custom Design HRESET_B not released 嗨,布莱斯 你能解释一下你修改了哪些步骤才做对了吗?目前我也遇到了类似的问题,使用的是定制的LS1046A主板。 Re: LS1046A Custom Design HRESET_B not released <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 感谢您之前的解答。 最后,我已经解决了 CPLD 代码中的电源时序问题。由于我之前的代码导致了这个问题,所以我重写了代码,现在问题已经解决了。 Re: LS1046A Custom Design HRESET_B not released <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 请创建一份技术案例,以便我能够查看处理器连接原理图。 Re: LS1046A Custom Design HRESET_B not released <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 我们已经将硬件绑定到使用硬编码的 RCW,而不是来自闪存的 RCW。 Re: LS1046A Custom Design HRESET_B not released <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 请使用数字示波器检查是否能从外部闪存读取 RCW。 Re: LS1046A Custom Design HRESET_B not released <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 你好, 谢谢你的回复。我已经确认以上所有物品都处于良好状态。关于您最后一点,我还有一个问题:这是上电复位序列完成的必要条件吗?正如我之前所说,我们无法观察到 RESET_REQ 信号,所以我认为我们无法执行 PBL。SerDes 参考时钟是执行 PBL 所必需的,还是在 PBL 设置系统时才需要的? 谢谢! Re: LS1046A Custom Design HRESET_B not released <meta http-equiv="Content-Type" content="text/html; charset=utf-8" /> 第一阶段检查请检查: 1) QorIQ LS1046A、LS1026A 数据表表 1 中明确提及的所有信号的 POR 水平。按总线列出引脚图。 2) HRESET_B 未被外部钳位 3) SerDes 参考时钟符合数据手册的要求。 如果问题无法解决,则更方便地将下一阶段的启动工作作为技术案例来执行: https://community.nxp.com/thread/381898
記事全体を表示
Coupon not valid for FRDM-MCXN236 NXP Website advertised this free board to get started . But the coupon code is still not working during checkout even though the product is in stock.  Evaluation Board Re: Coupon not valid for FRDM-MCXN236 Hello PLACEHOLDER7 In this case, please kindly send an email to our shopping cart team by [email protected]. The team is in charge of online orders. Thanks for understanding Becky
記事全体を表示
プロモーションクーポン こんにちは、 私のプロモーションクーポン「ADCWFBXT」がFRDM-MCXN236に有効でないのはなぜですか? プラモド・ジョグレカール [email protected] 開発ボード FRDMトレーニング Re: PROMO Coupon 私もFRDM-MCXN236のプロモーションクーポンを使うことができませんでした。 Re: PROMO Coupon クーポンコードADCWFBXTは2025年12月30日まで有効でしたのでご注意ください。当社のウェブサイトに記載されているとおり、 FRDMはイノベーションを推進します。費用は当社が負担します!   良い一日をお過ごしください。 Re: PROMO Coupon FRDM-MCXN236ボード用の他のクーポンはありますか?
記事全体を表示
PROMO Coupon Hi, Why is my promo coupon 'ADCWFBXT' not valid for the FRDM-MCXN236. Pramod Joglekar [email protected] Development Board FRDM-Training Re: PROMO Coupon Please note that the coupon ADCWFBXT was valid until December 30th, 2025. As stated at our website: FRDM to Innovate - On us!    Wishing you a nice day. Re: PROMO Coupon Even I am not able to use the promo coupon for FRDM-MCXN236. Re: PROMO Coupon Is their any other coupon available for FRDM-MCXN236 boards ?
記事全体を表示
S32K358 MBDT/Simulink – 将 SoC 存储在非易失性存储器中 您好,NXP团队, 我正在使用 RD-BESSK358BMU 板(S32K358 MCU)以及 MATLAB/Simulink 和 NXP MBDT。 我的板上运行着一个 EKF SOC 估算器。我需要定期将计算出的 SOC 保存到非易失性存储器中,以便在完全断电/开机后,可以读取最后存储的 SOC 并将其用作 EKF 的初始 SOC。 在 Simulink/MBDT 中,对于 S32K358,推荐的实现方式是什么? 我可以在 S32 配置工具中看到 Fee、MemAcc 和 Mem_43_InFls。这些模块是否适用于此目的? 您能否分享一些关于S32K358 Simulink/MBDT非易失性读/写的示例? 我找到了一些使用 EEPROM/FEE 的较早的 S32K 示例,但我特别想找到适用于 Simulink/MBDT 的 S32K358 的推荐解决方案。 谢谢。
記事全体を表示
S32K358 MBDT/Simulink – Store SOC in Non-Volatile Memory Hello NXP Team, I am using the RD-BESSK358BMU board (S32K358 MCU) with MATLAB/Simulink and NXP MBDT. I have an EKF SOC estimator running on the board. I need to periodically save the calculated SOC in non-volatile memory, so after a complete power OFF/ON, the last stored SOC can be read and used as the initial SOC of the EKF. What is the recommended way to implement this in Simulink/MBDT for S32K358? I can see Fee, MemAcc, and Mem_43_InFls in the S32 Configuration Tool. Should these modules be used for this purpose? Is there any S32K358 Simulink/MBDT example for non-volatile Read/Write that you can share? I found older S32K examples using EEPROM/FEE, but I am specifically looking for the recommended solution for S32K358 with Simulink/MBDT. Thank you.
記事全体を表示
S32K358 MBDT/Simulink – SOCを不揮発性メモリに保存する こんにちは、NXPチームの皆さん。 RD-BESSK358BMUボード(S32K358 MCU)をMATLAB/SimulinkとNXP MBDTで使っています。 ボード上でEKF SOC推定器を動作させています。計算されたSOCを定期的に不揮発性メモリに保存する必要があるため、完全な電源オフ/オン後、最後に保存されたSOCを読み取り、EKFの初期SOCとして使用できるようにします。 Simulink/MBDTでS32K358を実装する際の推奨される方法は何ですか? S32設定ツールでFee、MemAcc、Mem_43_InFlsが見えます。これらのモジュールをこの目的に使用すべきでしょうか? S32K358、不揮発性の読み書き(Read/Write)に関するSimulink/MBDTの例があれば教えてもらえますか? EEPROM/FEEを使用した古いS32Kのサンプルは見つかりましたが、Simulink/MBDTを使用したS32K358向けの推奨ソリューションを具体的に探しています。 ありがとう。
記事全体を表示
ZeroWattic Power Saver Reviews 2026 - Is Everything Really As Promised? ZeroWattic Power Saver Review 2026: Does This Device Really Help Reduce Electricity Waste? Rising electricity costs have made energy efficiency a priority for households and businesses. Many people are looking for simple ways to manage power consumption without replacing every appliance or making expensive electrical upgrades. This is where devices such as the ZeroWattic Power Saver have attracted attention. Presented as a compact power-saving solution, ZeroWattic is designed around the idea of improving the way electricity is used inside a home. The product packaging shown describes it as a device intended to address “dirty, chaotic current” and improve the flow of electricity through household wiring. But what exactly is ZeroWattic Power Saver, how is it supposed to work, and what should consumers know before purchasing one? In this detailed guide, we look at the product concept, potential benefits, installation considerations, limitations, and important questions buyers should ask before making a decision. Important: Product claims about electricity savings should be independently verified before relying on them for financial savings. Actual results can vary depending on the electrical system, appliances, usage patterns, tariffs, and other factors. Discover ZeroWattic Power Saver and Explore a Smarter Approach to Household Energy Management What Is ZeroWattic Power Saver? ZeroWattic Power Saver is marketed as a household electricity-management device. From the packaging, the product focuses on the quality and characteristics of electrical current flowing through a home's wiring. The basic concept is that certain electrical loads—particularly appliances containing motors, transformers, compressors, or switching electronics—can create electrical characteristics that are not always converted into useful work. Power-management products often attempt to address these characteristics through electrical components designed for power conditioning or power-factor correction. The ZeroWattic packaging specifically promotes the idea of reducing undesirable electrical effects and improving the flow of electricity through household wiring. For consumers, the key point is that power quality and actual electricity consumption are not necessarily the same thing. A device may affect certain electrical characteristics without automatically producing a large reduction in the kilowatt-hours recorded on a residential electricity meter. Therefore, buyers should look at the product's technical specifications and independently measurable results rather than relying only on broad marketing language. 🔌 Ready to Take Control of Your Electricity Usage? Learn More About ZeroWattic Today
記事全体を表示
ZeroWattic 节能器评测 2026 - 真的像宣传的那样好吗? ZeroWattic 节能器 2026 年评测:这款设备真的有助于减少电力浪费吗? 不断上涨的电费使得提高能源效率成为家庭和企业的首要任务。许多人都在寻找简单的方法来管理电力消耗,而无需更换所有电器或进行昂贵的电气升级。正因如此,像ZeroWattic 节能器这样的设备才引起了人们的关注。 ZeroWattic 是一款紧凑型节能解决方案,其设计理念是改善家庭用电方式。产品包装上显示,该产品是一种旨在解决“脏乱电流”并改善家用线路电流的设备。 但 ZeroWattic Power Saver 究竟是什么?它的工作原理是什么?消费者在购买前应该了解哪些信息? 在本详细指南中,我们将探讨产品概念、潜在优势、安装注意事项、局限性以及买家在做出决定前应该提出的重要问题。 重要提示:有关节电的产品声明在用于节省开支之前,应进行独立核实。实际结果可能因电力系统、电器、使用模式、电价和其他因素而异。了解 ZeroWattic 节能器,探索更智能的家庭能源管理方式 什么是 ZeroWattic 节能器? ZeroWattic Power Saver 是一款家用电力管理设备。从包装上看,该产品侧重于流经家庭线路的电流量的质量和特性。 基本概念是,某些电气负载(特别是含有电机、变压器、压缩机或开关电子元件的电器)会产生一些电气特性,而这些特性并不总是能转化为有用的功。电源管理单元产品通常试图通过专为电源调节或功率因数校正而设计的电气元件来解决这些特性。 ZeroWattic 包装专门宣传减少不良电气效应和改善家用线路电流流动的理念。 对于消费者而言,关键在于电能质量和实际用电量并不一定是一回事。设备可能会影响某些电气特性,但不会立即导致居民用电表记录的千瓦时数大幅减少。 因此,买家应该查看产品的技术规格和独立可衡量的结果,而不是仅仅依赖于宽泛的营销语言。 🔌 准备好掌控您的用电量了吗?立即了解更多关于 ZeroWattic 的信息
記事全体を表示
ZeroWattic Power Saver 2026 レビュー - 本当に約束通りなのか? ZeroWattic Power Saver 2026 レビュー:このデバイスは本当に電力の無駄を削減するのに役立つのか? 電気料金の高騰により、家庭や企業にとってエネルギー効率の向上は最優先事項となっている。多くの人々は、家電製品をすべて買い替えたり、高額な電気設備の改修を行ったりすることなく、電力消費を管理する簡単な方法を探している。こうした状況において、ZeroWattic Power Saverのような機器が注目を集めている。 コンパクトで省電力のソリューションとして提示されたZeroWatticは、**ホーム**内の電気利用方法を改善するという**アイデア**を中心に設計されています。展示されている製品パッケージでは、「汚れた混沌とした電流」を解決し、家庭用配線の電気の流れを改善することを目的とした装置と説明されています。 しかし、ZeroWattic Power Saverとは一体何なのか、どのように機能するのか、そして消費者は購入前に何を知っておくべきなのか? この詳細なガイドでは、製品のコンセプト、潜在的な利点、設置上の考慮点、制限、そして購入者が判断する前に尋ねるべき重要な質問について見ていきます。 重要: 電力節約に関する製品主張は、ファイナンシャル節約に頼る前に独立して検証すべきです。実際の結果は、電気系統、家電、使用パターン、料金表、その他の要因によって異なります。ZeroWattic Power Saverを発見し、より賢い家庭のエネルギーマネジメントアプローチを探りましょう ZeroWatticパワーセーバーとは何ですか? ZeroWattic Power Saverは家庭用電気マネジメントデバイスとして販売されています。パッケージからは、ホームの配線を流れる電流の品質と特性に焦点を当てています。 基本的な概念は、特定の電気負荷、特にモーター、トランス、コンプレッサー、またはスイッチング電子機器を含む機器が、必ずしも有用な仕事に変換されない電気的特性を生み出す可能性があるということです。パワーマネージメント製品は、電力調整や力率補正のために設計された電気部品を通じてこれらの特性を解決しようと試みることが多いです。 ZeroWatticパッケージは、望ましくない電気的影響を減らし、家庭用配線内の電力の流れを改善するという考えを特に推進しています。 消費者にとって重要なのは 、電力品質と実際の電力消費量が必ずしも同じものではないということです。装置は特定の電気特性に影響を与えることができますが、住宅用電力メーターに記録されるキロワット時の大幅な減少を自動的に生じさせることはありません。 したがって、購入者は広範なマーケティング言語に頼るのではなく、製品の技術的仕様や独立して測定可能な結果を重視すべきです。 🔌 電気使用量を管理する準備はできていますか?ZeroWatticについてもっと詳しく知りたい方はこちら
記事全体を表示