Multi Source Translation Content

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Multi Source Translation Content

ディスカッション

ソート順:
T2080RDBは、RCWとSERDESの関係を説明しています Re:T2080RDBそのドキュメントは、RCWとSERDESの関係を説明しています 「19.1.1.1.1」の項を参照してください。SerDes Protocols (SerDes 1 and SerDes 2)」を添付T2080RM.pdf
記事全体を表示
i.MX8MQ - How to control specific GPIO through i.MX GPIO Controller Driver Hi Teams, We have a GPIO as an input pin that we want to communicate it through i.MX GPIO Controller Driver. Can you give us example to set/get specific GPIO pin through i.MX GPIO Controller driver under Windows 10 21H2 ARM64? Thanks for you and all NXP Support Teams help! i.MX 8M | i.MX 8M Mini | i.MX 8M Nano Windows Windows 10 IoT Enterprise Re: i.MX8MQ - How to control specific GPIO through i.MX GPIO Controller Driver Hello,  Please refer to https://github.com/microsoft/Windows-iotcore-samples/tree/develop/BusTools/GpioTestTool Best regards, Salas.
記事全体を表示
GPIO commands not working: "device or resource busy" Hi everybody, I'm using iMX93QSB and i'm tryng to debug GPIO interface of the processor using prebuild linux image. I would like to change the P2_6 pin of the GPIO expander PCAL6524HEAZ which drives the selection pin fo the TMUX used on the board. Thanks to the driver I can see the GPIO expander as the gpiochip 4 and I should be able to move the pins by using libgpiod commands like: gpioset -t0 -c 4 22=1 .  But when I try to access to pin 22 (that is corresponding to P2_6) I receive the following message: so I checked the gpioinfo and I notice pin 22 is used by "consumer = ?": I cannot understand why isn't possible to change a gpio pin that's routed in order to be a selection pin. Can you help me? How can I change my selection mode from command line? Regards, Roberto Re: GPIO commands not working: "device or resource busy" Hello, I have not used device-tree-compiler to decompile .dtb in dts but I suggest you take a look on the next post, it could be helpful. Also, please follow the steps on Yocto user's guide  before use Devshell. Best regards. Re: GPIO commands not working: "device or resource busy" Hello @JorgeCas ,Thanks for answering, Is it possible to modify .dtb file within Linux shell? Someone on the internet suggests to use device-tree-compiler to decompile .dtb in dts, change what you need and then compile it again. But when I try to install with: sudo apt-get install device-tree-compiler, I receive: Can you help me please? Thanks in advance. Best regards, Roberto Re: GPIO commands not working: "device or resource busy" Hello,   That GPIO is used for shared GPIO mux on QSB board.   It is defined here.   To use it, you need to change the definition on that node to make it available.   Best regards.
記事全体を表示
How to obtain the lockstep status of the S32K342 chip core Hello:         I learned that the S32K342 chip is a lockstep chip, but my customers are obsessed with obtaining the lockstep status of this chip. Because they have functional security requirements, they must ensure that the lockstep function of the S32K342 chip is turned on, so I would like to ask how to obtain the lockstep status of this chip, the information stored in registers or flash memory.                                                                                                                                           Best regret. Re: How to obtain the lockstep status of the S32K342 chip core Thank you very much. This is the answer I want. Re: How to obtain the lockstep status of the S32K342 chip core Hi@xinglong Please take a look at the register:DCM_GPR “DCMROF19” register bit 29 (bit LOCKSTEP_EN): 0 = decoupled mode 1 = lockstep mode
記事全体を表示
Processor Expert for S32K146EVBを使用したI2Cスキャナー こんにちは、私はProcessor Expertを使用してS32K146EVBを使用してI2Cスキャナーに取り組んでいます。 I2Cを初期化でき、Acknowledgeを読んでいると問題が発生します。 私はあなたの親切な参照のために私のファイルを添付しました.. すぐにご連絡をお待ちしております。 @VaneB @Senlent 
記事全体を表示
提交NDA申请后一般多久可以签? 我已经在https://support.nxp.com/s提交了NDA申请(服务申请: 00624736),得到过一次答复说已经提交给法务了,但是过去1周了,没有进一步消息,也不清楚是不通过还是法务还没审核? 一般签这个NDA需要多长时间呢?
記事全体を表示
LTE Coexistence with IW416 Hi, Would like to check if LTE Coexistence is supported with IW416? Thanks, Pankaj Re: LTE Coexistence with IW416 hi Weidong, Can you please also calrify the LTE Coexistence for 88W9098 and IW610 chips? Thanks in advance. Thanks, Pankaj Re: LTE Coexistence with IW416 Dear @pankaj , Yes, LTE Coexistence is supported. Below is abstracted from datasheet, check it, please! 1. Coexistence descriptions in datasheet 2. Coexistence overview -- An application note  https://www.nxp.com/products/IW416 If you can't access the document, it means that you don't have access right. It is Secure File. you need these 2 steps to get authentication  from product manager. --NDA with NXP --Applying for access rights. Login nxp website--->My NXP Account--->Secure Files--->Filling out information following guidance---submit --->waiting for approval from product manager. Thanks! Regards, weidong
記事全体を表示
S32K342チップコアのロックステップステータスを取得する方法 こんにちは: S32K342チップがロックステップチップであることを知りましたが、お客様はこのチップのロックステップステータスを取得することに夢中になっています。機能的なセキュリティ要件があるため、S32K342チップのロックステップ機能がオンになっていることを確認する必要がありますので、このチップのロックステップステータス、レジスタまたはフラッシュメモリに保存されている情報を取得する方法を尋ねたいと思います。                                                                                                                                          最高の後悔。 Re:S32K342チップコアのロックステップステータスを取得する方法 ありがとうございました。これが私が欲しい答えです。 Re:S32K342チップコアのロックステップステータスを取得する方法 Hi@xinglong レジスターをご覧ください:DCM_GPR 「DCMROF19」 レジスタ ビット 29 (ビット LOCKSTEP_EN): 0 = デカップリング・モード 1 = ロックステップ・モード
記事全体を表示
USB0 host mode downstream ports Hello NXP Experts, on p57, Rev. 2.3 of LPC55S2X_LPC552X datasheet it states the following: Section 7.23.1.2 USB0 host controller: Features: "Two downstream ports" Could you please detail what this means? can two devices be connected to same PHY? where can i find more info either as a code or appnote? Thanks in advance! Re: USB0 host mode downstream ports Hello @diego_charles : Thanks a lot for clarification! Re: USB0 host mode downstream ports Hi @manuela_mendez  Thank you for your reply,  Bascially, the number of downstream ports indicated by the datasheet is the  number of physical downstream ports supported by the USB0 in  host controller mode. Below some screenshots of descriptions and diagrams that I found by checking  the USB 2.0 specification, please take a look at its terminology. Personally, I found this figure more explanatory.  Taking the information from above, I  like to see it this more  practical way: according to the spec and the DS specification , we should be able to connect to the host controller a  HUB with  two devices attached to it. Each device would be a downstream port, which upstreams data. I hope this helps, if you are facing any particular issues with your application and our LPC55xx MCU feel free create another thread and we will be happy to check. Diego
記事全体を表示
I2C Scanner using Processor Expert for S32K146EVB Hello I am working on I2C Scanner by using S32K146EVB using Processor Expert. I am able to initialize I2C and while reading the Acknowledge, it is giving a problem. I have attached my file for your kind reference.. I hope to hear from you soon.. @VaneB @Senlent  Re: I2C Scanner using Processor Expert for S32K146EVB Hi Nibesh, Sorry for not testing it for you in the previous question I2C Scanner using S32K146EVB-Q144. But as I mentioned there, since the LPI2C_init of S32K146_Project_LPI2C configure MCFGR1[IGNACK] to Ignore NACK by default, and its LPI2C_Transmit uses MTDR[CMD]=5 by default:101b  Generate (repeated) START and transmit address in DATA[7:0]. This transfer expects a NACK to be returned. So you can't judge the acknowledgement by polling MSR[NDF](NACK Detect Flag). Please try to test the following code: void LPI2C_Transmit (uint8_t address)/* Transmit ID and expects an ACK to be returned */ { LPI2C0->MTDR = (0x04<<8)|((address<<1)|0); } LPI2C_DRV_MasterInit(0, &lpi2c1_MasterConfig0, &lpi2c1MasterState); LPI2C0->MCFGR1 |= LPI2C_MCFGR1_AUTOSTOP_MASK; //Automatic STOP Generation        for(i=1; i<127; i++)        { //       LPI2C_DRV_MasterSetSlaveAddr(INST_LPI2C1, i, false);        LPI2C_Transmit(i);        delay(100);         if((((LPI2C0->MSR) & LPI2C_MSR_NDF_MASK) >> LPI2C_MSR_NDF_SHIFT)==true)         {         LPI2C0->MSR &= LPI2C_MSR_NDF_MASK;         LPUART_DRV_SendDataBlocking(INST_LPUART2, Space, sizeof(Space), TIMEOUT);         }         else         { sprintf( Buffer,"0x%X", i); LPUART_DRV_SendDataBlocking(INST_LPUART2, Buffer, sizeof(Buffer), 10000);         }        } Best Regards, Robin ------------------------------------------------------------------------------- Note: - If this post answers your question, please click the "Mark Correct" button. Thank you! - We are following threads for 7 weeks after the last post, later replies are ignored Please open a new thread and refer to the closed one, if you have a related question at a later point in time. -------------------------------------------------------------------------------
記事全体を表示
NDA 申請を提出してから署名を得るまでに通常はどのくらいの時間がかかりますか? https://support.nxp.com/s に NDA リクエストを送信しました (サービスリクエスト:00624736に申請したところ、法務部に提出済みとの返信をいただきましたが、1週間経っても何の連絡もありません。却下されたのか、法務部がまだ確認していないのか、はっきりしません。 このNDAに署名するには通常どのくらい時間がかかりますか?
記事全体を表示
USB0 主机模式下行端口 您好,恩智浦专家, 在第 57 页,修订版LPC55S2X_LPC552X 数据表 2.3 版指出以下内容: 第 7.23.1.2 节USB0 主机控制器:功能:“两个下游端口” 你能详细说明一下这是什么意思吗?两个设备可以连接到同一个 PHY 吗?我可以在哪里找到更多信息(例如代码或应用说明)? 提前感谢! 回复:USB0 主机模式下行端口 你好@diego_charles :非常感谢你的澄清!
記事全体を表示
使用处理器专家的S32K146EVB I2C扫描仪 您好,我正在使用 Processor Expert 使用 S32K146EVB 开发 I2C 扫描仪。 我能够初始化 I2C,但在读取确认时,出现了问题。 我已附上我的文件供您参考。 我希望很快收到您的回复。 @VaneB @Senlent
記事全体を表示
Network error on s32g QNX7.1 Dear NXP, I am running QNX7.1 on S32G-VNP-RDB2, but there are problems with the network. The NIC dwc0 is identified after the system starts, I configured a valid ip for it. But it can not ping other machines(return info: "ping: sendto: Host is down"), and no machine could ping the board. Could you please suggest, is there any other work that needs to be done here. Thank you for your support. Re: Network error on s32g QNX7.1 Hello, Check with QNX since this works with the NXP BSP, Regards
記事全体を表示
如何获取S32K342芯片内核的锁步状态 你好: 我了解到S32K342芯片是一款锁步芯片,但我的客户却痴迷于获得这款芯片的锁步状态。因为他们有功能安全的需求,必须保证S32K342芯片的锁步功能是开启的,所以想问一下如何获取这个芯片的锁步状态,寄存器或者闪存中保存的信息。 最好的遗憾。 回复:如何获取S32K342芯片核心的锁步状态 非常感谢。这就是我想要的答案。 回复:如何获取S32K342芯片核心的锁步状态 嗨@兴隆 请查看寄存器:DCM_GPR“DCMROF19” 寄存器位29(位LOCKSTEP_EN): 0 = 解耦模式 1 = 锁步模式
記事全体を表示
imx8mq - configure 4gb memory Dear Nxp engineers,  We have a design based on imx8mq with 3GB DDR - it's working fine.  Now we upgrade it to 4gb memory.  I have been following this link to apply the patch.  https://community.nxp.com/t5/i-MX-Processors/LGE-CTO-booting-failure-with-4G-DRAM-with-OPTE/m-p/1223113 In this link if apply patch and disable OP-TEE, according to the discussion in the link, it should work. But my board would still stuck in "Starting Linux..." Could you help to suggest the proper way to configure 4gb ddr? This is my patch: @@ -18,15 +18,12 @@ }; firmware { - optee { - compatible = "linaro,optee-tz"; - method = "smc"; - }; }; memory@40000000 { device_type = "memory"; - reg = <0x00000000 0x40000000 0 0xc0000000>; + reg = <0x0 0x40000000 0 0xc0000000>, + <0x1 0x00000000 0 0x40000000>; }; pcie0_refclk: pcie0-refclk { diff --git a/configs/imx8mq_evk_defconfig b/configs/imx8mq_evk_defconfig index 08bcb399b1f..0f51fb6ceef 100644 --- a/configs/imx8mq_evk_defconfig +++ b/configs/imx8mq_evk_defconfig @@ -163,10 +163,11 @@ CONFIG_SHA384=y CONFIG_EFI_VAR_BUF_SIZE=139264 CONFIG_EFI_IGNORE_OSINDICATIONS=y CONFIG_EFI_CAPSULE_AUTHENTICATE=y -CONFIG_OPTEE=y +CONFIG_OPTEE=n CONFIG_CMD_OPTEE_RPMB=y CONFIG_EFI_MM_COMM_TEE=y CONFIG_TEE=y CONFIG_EFI_ESRT=y CONFIG_EFI_HAVE_CAPSULE_UPDATE=y CONFIG_FIT_SIGNATURE=y +CONFIG_NR_DRAM_BANKS=2 \ No newline at end of file diff --git a/include/configs/imx8mq_evk.h b/include/configs/imx8mq_evk.h index 567e120e276..70b44999b6d 100644 --- a/include/configs/imx8mq_evk.h +++ b/include/configs/imx8mq_evk.h @@ -177,6 +177,8 @@ #define CONFIG_SYS_SDRAM_BASE 0x40000000 #define PHYS_SDRAM 0x40000000 #define PHYS_SDRAM_SIZE 0xC0000000 /* 3GB DDR */ +#define PHYS_SDRAM_2 0x100000000 +#define PHYS_SDRAM_2_SIZE 0x40000000 /* */ #define CONFIG_MXC_UART_BASE UART1_BASE_ADDR Re: imx8mq - configure 4gb memory Thanks Pengyong, this issue is resolved by useing ddr tool to generate new timing file Re: imx8mq - configure 4gb memory Hi @wenyong  You can use our DDR Config Tool configuration the ddr MT53E1G32D2FW parameters, Then the tool will generate the new timing.c file which you can use it compile the new uboot flash.bin file to boot your board. https://www.nxp.com/design/design-center/development-boards-and-designs/i-mx-evaluation-and-development-boards/config-tools-for-i-mx-applications-processors:CONFIG-TOOLS-IMX B.R Re: imx8mq - configure 4gb memory Hi @wenyong  OK, this can support 4GB DRAM, Please share your DDR datasheet and schematic file. I will help you configurate the DDR parameters. B.R Re: imx8mq - configure 4gb memory Hi pengyong,  We are using PN# MIMX8MQ6CVAHZAB Thanks, Wenyong Re: imx8mq - configure 4gb memory Hi @pengyong_zhang ,  We use MIMX8MQ6CVAHZAB. Re: imx8mq - configure 4gb memory Hi @wenyong  What is your i.MX8MQ SOC Part number? Because only Quad- A53 can support 4GB DRAM. B.R
記事全体を表示
S32K3 编译枚举,导致地址发生动态偏移 使用S32DS3.4进行编译,出现如下警告: c:/nxp/s32ds.3.4/s32ds/build_tools/gcc_v10.2/gcc-10.2-arm32-eabi/bin/../lib/gcc/arm-none-eabi/10.2.0/../../../../arm-none-eabi/bin/real-ld.exe: warning: c:/nxp/s32ds.3.4/s32ds/build_tools/gcc_v10.2/gcc-10.2-arm32-eabi/bin/../lib/gcc/arm-none-eabi/10.2.0/../../../../arm-none-eabi/lib/thumb/v7e-m+fp/hard\libc_nano.a(lib_a-memcmp.o) uses variable-size enums yet the output is to use 32-bit enums; use of enum values across objects may fail c:/nxp/s32ds.3.4/s32ds/build_tools/gcc_v10.2/gcc-10.2-arm32-eabi/bin/../lib/gcc/arm-none-eabi/10.2.0/../../../../arm-none-eabi/bin/real-ld.exe: warning: c:/nxp/s32ds.3.4/s32ds/build_tools/gcc_v10.2/gcc-10.2-arm32-eabi/bin/../lib/gcc/arm-none-eabi/10.2.0/../../../../arm-none-eabi/lib/thumb/v7e-m+fp/hard\libc_nano.a(lib_a-memcpy-stub.o) uses variable-size enums yet the output is to use 32-bit enums; use of enum values across objects may fail 此警告导致全局变量发生地址偏移,如何解决此问题?
記事全体を表示
USB0 ホスト・モード・ダウンストリーム・ポート こんにちはNXPの専門家、 p57、改訂版。LPC55S2X_LPC552Xデータシートの2.3には、次のように記載されています。 セクション 7.23.1.2USB0 ホスト コントローラー: 機能: "2 つのダウンストリーム ポート" これが何を意味するのか、詳しく説明していただけますか?2つのデバイスを同じPHYに接続できますか?コードまたはAppnoteとして、詳細情報はどこで入手できますか? よろしくお願いいたします! 日時:USB0ホストモードダウンストリームポート こんにちは@diego_charles:説明してくれてありがとう!
記事全体を表示
Does the MCU on the evaluation board S32K3X4EVB-Q172 support OTA? Hello, On the schematic of the evaluation board S32K3X4EVB-Q172, the MCU model is S32K344_172MAXQFP. In the S32K3XX data sheet, the mode is defined like this: P/S32K3NNXXT0MPASR.  In the S32K3xx reference manual, the OTA functionality is disabled in CUST_DEL Device Life Cycle. My question is, how to know if the MCU in the evaluation board supports OTA? Thanks! Crane     Re: Does the MCU on the evaluation board S32K3X4EVB-Q172 support OTA? Hi Crane, CUST_DEL: Device (that is, NXP IC) delivered to system integrator (that is, NXP’s customer) for ECU manufacturing and initial configuration. That is to say, the chip on your development board also has this life cycle by default. However, the OTA functionality can be enabled.  I suggest you download S32K3XX HSE and OTA Advance Training from secure file. Also take a look at S32K3_OTA_AB_SWAP_Demostration Best Regards, Robin ------------------------------------------------------------------------------- Note: - If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you! - We are following threads for 7 weeks after the last post, later replies are ignored Please open a new thread and refer to the closed one, if you have a related question at a later point in time. -------------------------------------------------------------------------------
記事全体を表示
How long does it usually take to get a signature after submitting an NDA application? I have submitted an NDA request at https://support.nxp.com/s ( Service Request: 00624736), and got a reply saying that it has been submitted to the legal department, but a week has passed and there is no further news. It is not clear whether it was rejected or the legal department has not reviewed it yet? How long does it usually take to sign this NDA? Re: 提交NDA申请后一般多久可以签? Hi @ZDDL  I am sorry for the inconvenience caused. My coworker is already helping you with this situation in the support ticket, so help me by communicating with her directly through that channel. B.R. VaneB
記事全体を表示