Hello,
On the schematic of the evaluation board S32K3X4EVB-Q172, the MCU model is S32K344_172MAXQFP.
In the S32K3XX data sheet, the mode is defined like this: P/S32K3NNXXT0MPASR.
In the S32K3xx reference manual, the OTA functionality is disabled in CUST_DEL Device Life Cycle.
My question is, how to know if the MCU in the evaluation board supports OTA?
Thanks!
Crane
Hi Crane,
CUST_DEL: Device (that is, NXP IC) delivered to system integrator (that is, NXP’s customer) for ECU manufacturing and initial configuration.
That is to say, the chip on your development board also has this life cycle by default.
However, the OTA functionality can be enabled.
I suggest you download S32K3XX HSE and OTA Advance Training from secure file. Also take a look at S32K3_OTA_AB_SWAP_Demostration
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------