I2C Scanner using Processor Expert for S32K146EVB Hello I am working on I2C Scanner by using S32K146EVB using Processor Expert. I am able to initialize I2C and while reading the Acknowledge, it is giving a problem. I have attached my file for your kind reference.. I hope to hear from you soon.. @VaneB @Senlent Re: I2C Scanner using Processor Expert for S32K146EVB Hi Nibesh,
Sorry for not testing it for you in the previous question I2C Scanner using S32K146EVB-Q144. But as I mentioned there, since the LPI2C_init of S32K146_Project_LPI2C configure MCFGR1[IGNACK] to Ignore NACK by default, and its LPI2C_Transmit uses MTDR[CMD]=5 by default:101b Generate (repeated) START and transmit address in DATA[7:0]. This transfer expects a NACK to be returned. So you can't judge the acknowledgement by polling MSR[NDF](NACK Detect Flag).
Please try to test the following code:
void LPI2C_Transmit (uint8_t address)/* Transmit ID and expects an ACK to be returned */ { LPI2C0->MTDR = (0x04<<8)|((address<<1)|0); }
LPI2C_DRV_MasterInit(0, &lpi2c1_MasterConfig0, &lpi2c1MasterState); LPI2C0->MCFGR1 |= LPI2C_MCFGR1_AUTOSTOP_MASK; //Automatic STOP Generation
for(i=1; i<127; i++)
{
// LPI2C_DRV_MasterSetSlaveAddr(INST_LPI2C1, i, false);
LPI2C_Transmit(i);
delay(100);
if((((LPI2C0->MSR) & LPI2C_MSR_NDF_MASK) >> LPI2C_MSR_NDF_SHIFT)==true)
{
LPI2C0->MSR &= LPI2C_MSR_NDF_MASK;
LPUART_DRV_SendDataBlocking(INST_LPUART2, Space, sizeof(Space), TIMEOUT);
}
else
{
sprintf( Buffer,"0x%X", i);
LPUART_DRV_SendDataBlocking(INST_LPUART2, Buffer, sizeof(Buffer), 10000);
}
}
Best Regards, Robin ------------------------------------------------------------------------------- Note: - If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored Please open a new thread and refer to the closed one, if you have a related question at a later point in time. -------------------------------------------------------------------------------
記事全体を表示