Hello NXP Community,
I am working on a bare-metal project with the following toolchain and software:
IDE: S32 Design Studio 3.6.0
MCAL: SW32K1_S32M24x_RTD_R21-11_3.0.0_D2503
Configuration Tool: EB Tresos Studio 29.0.0
Architecture: Bare-metal (no AUTOSAR OS, no third-party AUTOSAR BSW components, strictly NXP MCAL only)
My Goal:
I need a seamless and efficient workflow that allows me to:
Modify MCAL configurations in EB Tresos and regenerate code, with the changes automatically reflected in S32DS without manual copy-paste.
Manually develop and modify upper-layer BSW/ECAL code (e.g., my own ECU abstraction layer, complex drivers, application logic) directly within the S32DS project.
Compile the generated MCAL code and my manually developed code together in a single build successfully.
Questions:
Could you please clarify the officially recommended approach for this setup? Specifically:
What is the recommended mechanism to directly output and sync generated files from EB Tresos 29.0.0 into an S32DS 3.6.0 project structure?
What is the best practice for structuring the S32DS project folders (e.g., Generate, Mcal_Plugins, manual App/BSW folders) to ensure clean separation and combined compilation?
Could you kindly provide or point me to any professional guidance documents, application notes, or step-by-step tutorials (such as "How to import RTD EB project into S32DS") that describe this exact workflow for the R21-11 RTD MCAL? Any official documentation would be highly appreciated.
Thank you for your time and guidance.
Hi,
The available S32K3 AUTOSAR MCAL RTD Based Tresos Training provides useful guidance on working with an EB tresos project and RTD resources, including code generation and building the complete project using GNU Make from the command line:
S32K3xx AUTOSAR MCAL RTD BASED TRESOS_TRAINING
There is no automatic synchronization/integration that directly imports EB tresos generated files into an S32DS project. The generated configuration and required RTD resources need to be incorporated into the S32DS project/build structure accordingly, while your manually developed application/BSW sources can be maintained separately.
As a practical reference for this approach, the following NXP Community article demonstrates how an RTD EB tresos project can be integrated into S32DS:
[S32K3 Tools Part] How to import RTD EB project into S32DS
Please note that this Community example uses an S32K3 RTD release, so some paths and project settings may differ from the S32K1/S32M24x RTD 3.0.0 package, but the overall integration concept is applicable.
BR, Petr