2416632_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2416632_en-US

2416632_en-US

Can LPC55S0x CANFD support 1Mbps (arbitartion stage) and 8Mbps(data stage)

Hi NXP,

      Can LPC55S0x support 1Mbps in arbitration stage and 8Mbps in data stage ?

      I can't find in LPC55S0x datasheet.


     Thanks very much.

LPC55xxRe: Can LPC55S0x CANFD support 1Mbps (arbitartion stage) and 8Mbps(data stage)

Hi Harry,

      Got it.

      Thanks.

Re: Can LPC55S0x CANFD support 1Mbps (arbitartion stage) and 8Mbps(data stage)

Hi @jimmyli 

Yes— the LPC55S0x CAN-FD controller can be configured for 1 Mbit/s arbitration and 8 Mbit/s data , provided the MCAN functional clock is 96 MHz and the external CAN-FD transceiver and physical network support 8 Mbit/s.

The reason this is not listed directly in the datasheet is that the bit rates are derived from the MCAN clock and the NBTP / DBTP timing registers rather than specified as a fixed maximum. The CAN clock can use main_clk with CANCLKDIV = 0 (divide-by-1), and the LPC55S0x maximum clock frequency is 96 MHz.

BR

Harry

タグ(1)
評価なし
バージョン履歴
最終更新日:
火曜日
更新者: