I downloaded the official HSE installation example, but after running it, I found that HSE failed to install. The program gets stuck in the `while ( FALSE == HSE_CheckStatus(HSE_STATUS_INIT_OK) );` loop. I'm at a loss and need help on how to successfully install HSE. The attached file is the official example; I downloaded it, changed the `.project` file to `S32K312`, and disabled the `baf` file in the linker script. I didn't modify anything else.
Hi
I suggest you obtain the latest s32k3_hse_lib_rtd400hf01_20260427.7z from the distributor FAE and test it again. The new version fixes some bugs found in older versions.
According to section " 2.2 Version Number Details " of SBAF_S32K312_0_0_15_0_ReleaseNotes.pdf and the value shown in your screenshot at 0x4039C020 - 0x4039C027, it appears that AB_SWAP firmware was previously installed? If FULL_MEM was installed, the value at 0x4039C020 - 0x4039C027 should be 000D0000 000F0006.
However, what I see in your attached project is S32K312_0_2_40_0_HSE_FULL_MEM. I'm a bit confused about whether you need to install FULL_MEM or the HSE FW for AB_SWAP? Please check which build option you selected for the HseLib_HseFwInstall_Rtd400 project.
Please note that it is not possible to revert from AB_SWAP to FULL_MEM.
The screenshot you provided shows 0x4039C028=0xC0 bit0=0, meaning SBAF failed to boot HSE FW. It appears the HSE FW firmware is corrupted. You'll likely need to refer to MU Restore FW_EN.pdf to restore HSE FW using MU.
Please also refer to the manual s32k3_hse_lib_rtd400hf01_20260427\Doc\ S32K3_HSE_LIB_UserGuide.pdf . I didn't understand " blocked the baf file in the linker script ". Does it refer to page 19/51, section 3.3 of that document? .3In the "Build configuration - Settings of Linker" section, what about the file s32k3xx_flash_full_mem_0_2_40_0.ld? After installing SBAF_S32K312_0_0_15_0.exe, the path is C:\NXP\SBAF_S32K312_0_0_15_0\bin\s32k312_Secure_Baf_0.13.0_0.15.0.6_pb230804.bin.pink. This file does not need to be commented out.
Best Regards,
Robin