2375446_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2375446_en-US

2375446_en-US

IMX9596 and IMX9594 BSP compatibility

Based on the IMX95 specification, it seems that the only difference between IMX9594 and IMX9596 is the CPU cores. Are any BSP code changes required to support IMX9594? 


My BSP Code base is "Walnascar, imx-6.12.34-2.1.0.xml"

MACHINE=imx95evk DISTRO=fsl-imx-wayland source ./imx-setup-release.sh -b build-imx95

Re: IMX9596 and IMX9594 BSP compatibility

Hi @pengyong_zhang 

Thanks for your feedback.

So the same image can work on imx9594 and imx9596. Is that correct?



Re: IMX9596 and IMX9594 BSP compatibility

Hi @avery 

For the IMX9594 and IMX9596, no changes to the BSP code are required.

B.R

Re: IMX9596 and IMX9594 BSP compatibility

Hi @avery 

Yes, correct.

B.R

Tags (1)
No ratings
Version history
Last update:
‎06-06-2026 02:35 AM
Updated by: