2350607_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2350607_en-US

2350607_en-US

I want to use multiple can rx and send with different message Id

I want to use multiple Can Rx messages and I need to send same messages through different id’s. If anyone has working model please share here

Re: I want to use multiple can rx and send with different message Id

Hello @Sachinkumarar15,

There is an existing example inside the RTD package for a simple FlexCAN configuration, along with some additional ones in our community:

You can modify them to receive and transmit multiple IDs. For Rx, simply modify the Rx filter, and for Tx, you can re-use the same Tx data and change the msg_id. 

Best regards,
Julián

Tags (1)
No ratings
Version history
Last update:
‎04-15-2026 02:55 AM
Updated by: