2342166_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2342166_en-US

2342166_en-US

Which driver package needs to be installed on S32DS for BmsTPL3SLE2EConfig configuration

https://community.nxp.com/t5/S32K-Knowledge-Base/S32K344-MC33664-MC33775-RTD-3-0-0-BMS-SDK-1-0-2/ta-... 

RTD 3.0.0 : BMS SDK 1.0.2

Hi,I am using the program in the link for BMS testing, as shown in the attached image 1. Which installation package needs to be installed to modify the BmsTPL3SLE2EConfig variable? Can you provide it to me?
I followed the code in image 2 to drive the library, but it still doesn't display!

Re: Which driver package needs to be installed on S32DS for BmsTPL3SLE2EConfig configuration

Hi

After install SW32K3_BMS_SL_SDK_4.4_R21-11_1.0.2_DEMO_updatesite_D2401.zip the BMS_TPL3_SL_E2E will be able to be added to the project.

If you configured BMS_TPL3_SL_E2E using the S32 Configuration Tool, you would see `/generate/include/CDD_Bms_TPL3_SL_E2E_Cfg.h` folder.

However, that project did not add BMS_TPL3_SL_E2E; instead, it added the file directly to `MC33775_MC33664_example_S32K344_DS/src/lib/bms_lib.c`.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

-------------------------------------------------------------------------------

Tags (1)
No ratings
Version history
Last update:
‎03-31-2026 04:27 AM
Updated by: