2312617_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2312617_en-US

2312617_en-US

About flashing RCW on T1024 custom board
Hi,

I am trying to flash a pre-configured RCW file onto the flash memory (starting at 0xE800_0000) of a custom-built T1024 board using a CodeWarrior TAP. Since the flash is currently empty and lacks an RCW, is it possible to write the RCW.bin file data using the CodeWarrior TAP in this state? I would appreciate it if you could provide any relevant reference documentation or examples regarding this process.

Thansk in adnvace.

BR.
Jinwon
Re: About flashing RCW on T1024 custom board

Thanks for your answer and I have one more question. Is it possible to set RCW using Codewarrior tool except hard-coded mode? I found '8.2 Using a JTAG configuration file to override RCW' in Targeting_PA_Porcessors.pdf, one of Codewarrior documents but I have no idea how to adjust this in my custom board with blank flash(no rcw). Thanks in advance.

Re: About flashing RCW on T1024 custom board

Yes, that is possible. Set the RCW into hard-coded mode, and then please kindly follow the AN4948.

Flash Programmer for CodeWarrior Power Architecture

Thanks

Re: About flashing RCW on T1024 custom board

JTAG configuration files available with CodeWarrior Installation

(CWInstallDir\PA\PA_Support\Initialization_Files\jtag_chains) can be used to override Reset Configuration

Word (RCW) for the T1024.

You could adjust one T1024rdb file per your customer board.

But the the RCW1 and RCW 2 could not be adjusted.

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎02-07-2026 03:26 AM
更新者: