Thanks for your answer and I have one more question. Is it possible to set RCW using Codewarrior tool except hard-coded mode? I found '8.2 Using a JTAG configuration file to override RCW' in Targeting_PA_Porcessors.pdf, one of Codewarrior documents but I have no idea how to adjust this in my custom board with blank flash(no rcw). Thanks in advance.
Yes, that is possible. Set the RCW into hard-coded mode, and then please kindly follow the AN4948.
Flash Programmer for CodeWarrior Power Architecture
Thanks
JTAG configuration files available with CodeWarrior Installation
(CWInstallDir\PA\PA_Support\Initialization_Files\jtag_chains) can be used to override Reset Configuration
Word (RCW) for the T1024.
You could adjust one T1024rdb file per your customer board.
But the the RCW1 and RCW 2 could not be adjusted.