2292359_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2292359_en-US

2292359_en-US

Need working RTD version for S32 DS 3.6.4 with sample CAN application for S32K344

Hello, 

We just received multiple EVBs: https://www.nxp.com/design/design-center/development-boards-and-designs/MR-CANHUBK344

We want to test out each board for working CAN interfaces. For this purpose please point to working CAN example projects and RTD version which have been tested. I am not interested in loopback examples, but full CAN example which demonstrate RX and TX on the given board.

Thanks!

Re: Need working RTD version for S32 DS 3.6.4 with sample CAN application for S32K344

Hi,

there is direct "IEEE1722 demo app" demo example for this board available from its web page. But it was designed in S32DS3.4 and RTD2.0.0. You can simple refer to it. Most probably this will need to be ported, if you want to use latest S32DS, not sure of the RTD version you have. There was some successful port to S32DS3.5 and RTD300; https://community.nxp.com/t5/S32K/Porting-MR-CANHUBK344-IEEE1722-to-work-with-newer-S32DS-3-5-and/td... 

Simple CAN demo for FlexCAN0 is posted on https://community.nxp.com/t5/S32K-Knowledge-Base/RTD600-MCAL-amp-IP-S32K3X4EVB-T172-FlexCAN-Example-...
This should work on MR-CANHUBK344 as well, only check/modify the pin used for CAN0 EN/STB_N pins.

BR, Petr

Tags (1)
No ratings
Version history
Last update:
‎01-14-2026 03:29 AM
Updated by: