zuozuo_0-1767950109136.png
I was able to successfully conduct the CAN communication connection test in Figure 1, but after clicking OK, the fault as shown in Figure 2 occurred. How can I solve this problem?
zuozuo_1-1767950217655.png
In addition, I have used mbdt for freemaster development on S32K344, but I have not succeeded in polling mode CAN communication. Is it not supported? If it is supported, could you provide me with a sample, preferably for the S32K3 series
Now I have also implemented the polling mode and tested the connection of the can based freemaster. The effect is the same as the above picture. I will continue to seek help
Hi @zuozuo,
Are you using the MATLAB or S32 Design Studio as your primary development environment ?
In the later case - did you try the example applications that come with FreeMASTER Driver Update site ?
In case you are using MATLAB, a dedicated team is handling the MatLAB Toolbox and I will move your query to MBDT community space.
quickly ran from another computer with an earlier version of the pc side software and it worked fine. so i manually copied the connection string to the Option field and it worked. so the issue is either on the 1.16.0 or the PC admin previlage..
Hello,
one thing to try is to re-register the CAN communication plug-in in your system. Please close the FreeMASTER, and navigate to installation location. Then run the register.bat "As administrator". See more details in one of the earlier posts in this forum.
MichalH_0-1768547086259.png
Regards,
Michal
Hi, Michal,
thanks for the hint but it does not seem to work. by pasting a plain text string i could open the port. the computer that i had an older version of Freemaster 3.2 no longer works after i upgraded it to the latest version. i ran the register.bat as admin but the same error message appears. now two computers give me the same error.
I use the mbed toolchain to generate the underlying driver code for freemaster. Currently, both polling mode and interrupt mode can successfully connect with the host computer, and there are no issues with the slave computer. The only problem is that the freemaster host computer cannot save its own configuration options in the freemaster host computer project。
Hello the CAN plugin version 1.16.0 (in FreeMASTER 3.2.6.3) indeed adds the CAN-FD support for ZLG and some other vendors. It also adds support for the new ZLG ZCAN library. After the registrer.bat has been run, we can be sure the plug-in is correctly registered in the system.
I cannot replicate the issues you are facing. The connection string for the ZCAN devices appears normally in my case: drv=ZCAN;port=1;bitrate=500000;cmdid=0x7aa;rspid=0x7aa;tmo=500
MichalH_1-1768808840834.png
Please try the following:
Please let me know if it shows the error in all 3 cases.
Thanks,
Michal
Hello,
we are trying to analyze and resolve the issue, but unfortunately we were not able to replicate it on any of our test platforms. Please use the manually-edited connect string until this is fixed.
One question: when ZLG/ZCAN driver is selected, does the error appear when you press the CANCEL button in the plug-in dialog?
Thanks,
Michal
Hello,
we have identified the problem in FreeMASTER CAN plug-in and we are working on a fix. It appeared the plug-in has internally depended on Kvaser CAN driver and was not working correctly when Kvaser software was missing. It appears the Kvaser files are required even if using ZLG or any other CAN interface.
Before the fix is released in the upcoming FreeMASTER 3.2.7, a quick workaround is to install the latest Kvaser driver pack to your Windows system. You can download the Kvaser drivers here.
Thanks to all of you who had reported the issue and described the symptoms. Please reply to this message if installing the latest Kvaser drivers does not help to resolve the issue.
Thanks,
Michal
Hello,
theoretically yes, you may need to install Kvaser drivers even in case you use a PEAK device. The dependency on some Kvaser files causes the Plug-in configuration dialog to fail when creating a connection string regardless of the device selected.
It may happen by some lucky coincidence that the issue will not appear with PEAK or other devices, but if it does, installing the Kvaser driver shall always help.
This issue will be fixed in future FreeMASTER version.
Regards,
Michal
Note that the version 3.2.7 has been released. The issue discussed in this thread shall now be fixed.
Regards,
Michal