2263320_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2263320_en-US

2263320_en-US

Unable to remove write protection on NTAG213 after enabling password protection (AUTH0/ACCESS)

Hello NXP Team,

I am working with NTAG213 tags using the PN7160 NFC controller and the NXP Linux nfcDemoApp.

What I have done successfully:

  1. I modified the nfcDemoApp (main.c) to enable write-only password protection on NTAG213 by configuring:

    • PWD

    • PACK

    • AUTH0

    • ACCESS (PROT = 0)

  2. The write protection works correctly:

    • Mobile NFC apps cannot write anymore

    • Writing is possible only after sending PWD_AUTH from my application

    • Reset AUTH0 to 0xFF

    • Clear ACCESS

    • Re-write configuration pages

      I also enabled write protection on another NTAG213 using NXP NFC TagInfo / NFC Tools app, and that also worked as expected.

      Problem I am facing:

      Now I am unable to remove the write protection in both cases:

      • Using my own code (nfcDemoApp)

      • Using NXP NFC Tools / TagWriter mobile apps

      Even after authenticating with the correct password (PWD_AUTH), attempts to: are failing .

    My understanding:

    From the NTAG213 datasheet, I understand:

    • PWD_AUTH should allow writing to protected pages during the RF session

    • After authentication, it should be possible to modify AUTH0 and ACCESS

    • NTAG213 does not have permanent lock bits for password protection (unlike lock bytes)

    However, in practice, I am unable to revert the tag back to an unprotected state.

    Questions:

    1. Is it officially supported to remove or disable password-based write protection on NTAG213 after it has been enabled?

    2. Are AUTH0 and ACCESS pages writable after successful PWD_AUTH, or are they permanently protected once set?

    3. Is there a recommended sequence to restore NTAG213 to a writable (unprotected) state?

    4. Can NXP NFC Tools / TagWriter remove password protection on NTAG213, or is custom raw command handling required?

    5. Is full reset (RF session reset / power cycle) required after authentication to modify configuration pages?

    Any guidance or clarification from the NXP team would be very helpful.

    Thank you for your support.

    Best regards,
    Niranjan





Re: Unable to remove write protection on NTAG213 after enabling password protection (AUTH0/ACCESS)

I use the RFIDDiscover. It is able to change the settings in configuration page to remove the protection.

Tags (1)
No ratings
Version history
Last update:
‎12-25-2025 02:28 AM
Updated by: