2197690_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2197690_en-US

2197690_en-US

LS1046A 2.5G SGMII

Hi,

Is the 2.5G SGMII MAC interface on the LS1046A an OC-SGMII interface. I am trying to determine if 2500Base-X is the correct medium for this MAC interface.

On the LS1046A reference deisgn board the 2.5G SGMII link is connected to an AQR113 part from Marvell. However, the AQR113 datasheet does not mention 2.5G SGMII, so I am trying to understand how this works?

Re: LS1046A 2.5G SGMII

Hello,

It is because the AQR113 from MARVELL is compatible with 2.5GBASE-T

Re: LS1046A 2.5G SGMII

I do agree with your statement, but how does it work with the AQR113 part from Marvell?

Re: LS1046A 2.5G SGMII

Hello,

The LS1046A MAC interface uses 2.5G SGMII, not 2500Base-X.

Re: LS1046A 2.5G SGMII

Hi,

So the connection between the LS1046A and the ARQ113 on the LS1046A reference design board is XFI, and not SGMII 2.5G, or is it both capable?

ddnxpcom_0-1764701717664.pngddnxpcom_0-1764701717664.png


Re: LS1046A 2.5G SGMII

It is both capable. Please refer to the link below:

https://community.nxp.com/t5/Layerscape/LS2088A-SerDes-XFI-amp-2-5G-Query/m-p/1607421 

标记 (1)
无评分
版本历史
最后更新:
‎12-09-2025 03:29 AM
更新人: