2181198_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2181198_en-US

2181198_en-US

LMT101ENMFWD-ACD LCD 10.1'' HDMI with i.MX 8M Plus EVK Board

Hi, 

i am using LMT101ENMFWD-ACD LCD 10.1" with the i.MX 8M Plus EVK Board through HDMI connection. 

i have flashed the i.MX 8M Plus EVK with LF_v6.12.34-2.1.0_images_IMX8MPEVK.zip image


When the board boots up, the default resolution causes the content on the display to be squished.

i tried to update the weston.ini file but no impact happens. 


could you please tell me step by step how to update the resolution?


thanks

Eslam

Graphics & Displayi.MX 8M | i.MX 8M Mini | i.MX 8M NanoRe: LMT101ENMFWD-ACD LCD 10.1'' HDMI with i.MX 8M Plus EVK Board

Hello,

You may refer to the following community document if you are using HDMI port it is pretty straight forward:
https://community.nxp.com/t5/i-MX-Processors-Knowledge-Base/How-to-change-the-HDMI-pixel-clock-and-c...

Hope this helps,
Best regards/Saludos,
Aldo.

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 05:42 PM
Updated by: