2150009_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2150009_en-US

2150009_en-US

Blinking LED Example on S32K14WEVB-Q064 (RTM 2.0.0)

Hi,

I'm creating and testing  a 'Blinking LED Example' project on S32K14WEVB-Q064 reference board refering to the follwoing url:
https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/HOWTO-Create-the-Blinking-LED-example-...

There is no problem with creating the project, but when running in debug mode, execution stops at the CLOCK_DRV_Init function. Are there any separate clock or pin map settings required for the S32K14WEVB-Q064 reference board?


Re: Blinking LED Example on S32K14WEVB-Q064 (RTM 2.0.0)

Thank you for your reply and I have more questions about this.

I'm planning to develop the firmware update function via CAN. I found the solution, Unitfied bootloader(https://community.nxp.com/t5/S32K-Knowledge-Base/Unified-bootloader-Demo/ta-p/1423099). And I tried to build this solution and found that it's possible to do it on the specific S32DS(2018, RTM 2.0.0). 

My questions are

- Is it impossible to proceed with development using the current build environment(2018, RTM 2.0.0)?
- In the version you mentioned, is there any solution or example code we can refer to for implementing firmware updates based on CAN communication?

I appreciate in advance.

Re: Blinking LED Example on S32K14WEVB-Q064 (RTM 2.0.0)

Thank you for your interest in our products and for contributing to our community.

For development with S32K144W (or any other S32K1 derivative) we recommend to use the latest S32DS and RTD versions:

• S32 Design Studio 3.6.3 – Windows/Linux
• S32K1_S32M24X Real Time Drivers AUTOSAR R21-11 Version 3.0.0

To download IDE, go to S32 Design Studio for S32 Platform page -> Downloads ->
S32 Design Studio 3.6.3 – Windows/Linux

To download RTD, go to S32K1 page -> Design Resources -> Software-> Real-Time Drivers for S32K1 -> Automotive SW - S32K1_S32M24x - Real-Time Drivers for Cortex-M

Please check before Release Notes for installation flow/details to each SW.

Once you have installed SW, you could refer to project examples:

_Leo__0-1754956643349.png

I hope this information is helpful. Feel free to reach out if you have any further questions using Real-Time Drivers (RTD).

Re: Blinking LED Example on S32K14WEVB-Q064 (RTM 2.0.0)

For your reference, I chose this S32DS version to use Unified bootloader demo(https://community.nxp.com/t5/S32K-Knowledge-Base/Unified-bootloader-Demo/ta-p/1423099). 

Re: Blinking LED Example on S32K14WEVB-Q064 (RTM 2.0.0)

Please refer to my answer as belows. I appreciate in advance.


1) version of S32DS

S32 Design Studio for ARM Version 2018.R1


2)debug probe (e..g. onboard OpenSDA, external PEmicro multiling, segger....)

onboard OpenSDA


3) can you post a screenshot showing the code at CLOCK_DRV_Init() ideally including disassembly View.
attached a screen catpture

screencapture-CLOCK_DRV_INIT.png



Re: Blinking LED Example on S32K14WEVB-Q064 (RTM 2.0.0)

Hi, 

Could you provide us with more details?

1) version of S32DS

2)debug probe (e..g. onboard OpenSDA, external PEmicro multiling, segger....)

3) can you post a screenshot showing the code at CLOCK_DRV_Init() ideally including disassembly View.

Thanks,

Stan



Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 06:10 PM
Updated by: