How should the ld file be modified in the bootlouder project for S32K396s, is there a bootlouder example for K396?
Hello,
1. Unified Bootloader Demo for S32K3 Series
NXP provides a Unified Bootloader Demo that supports the S32K3 family, including the S32K396. This demo includes:
You can find the official post and download links here: Unified Bootloader Demo on NXP Community.
https://community.nxp.com/t5/S32K-Knowledge-Base/Unified-bootloader-Demo/ta-p/1423099
2. S32 Design Studio (S32DS) and RTD
To work with the bootloader example, you’ll need:
You can install these via the S32DS Extensions and Updates menu. Once installed, you can create a new project from example templates, such as:
More setup details are available in the Getting Started Guide for S32K396-BGA-DC1
Best regards,
Peter