2110377_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2110377_en-US

2110377_en-US

S32K3 memacc works on pflash causes hardfault when MEM_43_INFLS_AC_LOAD_ON_JOB_START is on

S32K3 memacc works on pflash causes hardfault when MEM_43_INFLS_AC_LOAD_ON_JOB_START is on

the data in the ram is totally same with the code in pflash

qimaomarvin_0-1749035661787.png

qimaomarvin_0-1749035771148.png


Re: S32K3 memacc works on pflash causes hardfault when MEM_43_INFLS_AC_LOAD_ON_JOB_START is on

Hi,

have you solved this issue?

I have the same behaviour, any suggestions?

Thanks a lot!

回复: S32K3 memacc works on pflash causes hardfault when MEM_43_INFLS_AC_LOAD_ON_JOB_START is on

Hi @qimao-marvin,

Can you specify the RTD revision and the S32K3xx part number?

Or can you share the whole project?


Thank you,

BR, Daniel

回复: S32K3 memacc works on pflash causes hardfault when MEM_43_INFLS_AC_LOAD_ON_JOB_START is on

Because the address i try to erase and prohran in at the bank of the functiob, the 0x400000 - 0x500000 is the one bank, but even i put the code in the ram ,it caused the hardfault too,however ,if i erase at the 0x500000,the function runs well

Re: S32K3 memacc works on pflash causes hardfault when MEM_43_INFLS_AC_LOAD_ON_JOB_START is on

Hi @qimao-marvin,

Can you specify the S32K3xx part number and the sector you program?

Can you share the project?

Regarding the hardfault, can you find more information about the fault?

Follow these guidelines:

https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K312-HARDFAULT-Handling-Interrupt-DS3-5-...

https://community.nxp.com/t5/S32K-Knowledge-Base/How-To-Debug-A-Fault-Exception-On-ARM-Cortex-M-V7M-...

https://community.nxp.com/t5/S32K-Knowledge-Base/Fault-handling-on-S32K14x/ta-p/1114447


BR, Daniel


Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 06:46 PM
Updated by: