2092019_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2092019_en-US

2092019_en-US

Software reset error when adapting TJA1120 driver to linux 5.15, error code -110

I'm having problems with software reset when adapting TJA1120 driver (from Linux 6.6) to Linux 5.15 with error code -110, I'm not sure about the cause as well as I don't know how to fix this problem.

I refer to this post NXP_C45_TJA11XX Driver Soft Reset Issue, made changes to nxp_c45_soft_reset, but it has no effect, the code is as follows.

static int nxp_c45_soft_reset(struct phy_device *phydev)
{
int ret;

ret = phy_write_mmd(phydev, MDIO_MMD_VEND1, VEND1_DEVICE_CONTROL,
DEVICE_CONTROL_RESET);
if (ret)
return ret;

usleep_range(2000, 2050);

return phy_read_mmd_poll_timeout(phydev, MDIO_MMD_VEND1,
VEND1_DEVICE_CONTROL, ret,
!(ret & DEVICE_CONTROL_RESET), 20000,
240000, true);
}:

Error.

[ 6.188117] sunxi-mdio 4500048.mdio0. sunxi_mdio_probe() BEGIN
[ 6.265731] sunxi-mdio 4500048.mdio0. phy id: 0x001bb031, adr: 0x1b, device: 4500048.mdio0-mii:1b, DRIVER: NXP C45 TJA1120
[ 6.278218] sunxi-mdio 4500048.mdio0. sunxi_mdio_probe() SUCCESS
[ 47.166283] NXP C45 TJA1120 4500048.mdio0-mii:1b:. nxp_c45_soft_reset failed: -110

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 09:13 AM
更新者: