2084966_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2084966_en-US

2084966_en-US

NXP FreeRTOS library

hi,

i wanna build a library using NXP FreeRTOS.


so let me know about the method to make a library with my function.

(like myLibrary.h and myLibarary.a)


thanks.


using software configuration

1) S32DS.3.5_b220726_win32.x86_64.exe
2) SW32_S32DS_3.5.8_D2311 package
3) SW32_S32DS_OfflineDevPack_3.5.0_D2207 package
4) SW32K3_RTD_4.4_3.0.0_P01_D2303_DS_updatesite package
5) NXP FreeRTOS 10.0.5 package

*System Clock : use default clock (peripheral - os - freertos - General option)


Re: NXP FreeRTOS library

Hi @jwjung 

For guidance on creating and adding a library in S32 Design Studio. I recommend taking a look at the following links, which provide detailed instructions that might be useful for you:

How to create a lib file and add it to another project with S32DS

HOWTO: Add a static library file into S32DS GCC project

Check them out and see if they help! If it is not quite what you are looking for or you have more questions, just let me know. 


BR, VaneB

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 01:04 PM
更新者: