Hi, I can not find S32K1xx SDK/RTD package in S32DS Extensions and Updates.
Where should I look for it ?
Thanks!
Hi
Please offline install S32K1 RTD by refer to the step 4 of HOWTO: offline install S32K1 RTD 2.0.0 in S32DS v3.5.
I installed the latest S32K1 RTD 2.0.0 QLP1 in S32DS v3.6.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------