2054398_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2054398_en-US

2054398_en-US

Why are NXP's power management ICs (PMIC/SBC) ideal for automotive microcontrollers (S32 series)? (Japanese blog)

The S32 microcontroller is a series of microcontrollers (MCUs) from NXP designed for automotive applications.

An automotive power management IC (PMIC) or system basis chip (SBC) suitable for the S32 microcontroller must have a wide range of functions beyond simply supplying power supply voltage, including supporting functional safety, power sequence control, and low-power operation.

Here, we will explain four benefits of using NXP's power management IC (PMIC/SBC) using the example of connecting to an NXP S32 microcontroller.

NXP PMIC MCU.jpg


Benefit 1: Support for functional safety design

Automotive MCUs and PMIC/SBCs must transition to a safe state when a system failure occurs. For this purpose, we support functional safety design as a system.

ISO 26262 compliant

ISO 26262 is an international standard for ensuring functional safety in automotive electronic control systems. This standard defines processes to reduce risks to drivers and passengers in the event of a system failure. Automotive electronic controls that require functional safety compliance are required to comply with ISO 26262.

ASIL (Automotive Safety Integrity Level)

This is a risk classification system defined in ISO 26262, and is an index for evaluating the safety of systems and components. It is classified into four levels, from ASIL-A to ASIL-D, with ASIL-D being the highest risk level. The higher the risk level, the greater the demands on functional safety.

・Reference article: Why are microcontrollers considered functional safety compliant? (Japanese blog)

Safety goals required for PMIC/SBC

To achieve safety goals, the PMIC/SBC must have the following functions:

- Monitoring of power supply voltages related to safety functions (such as the MCU core power supply) [Voltage Supervisor function in the diagram]

- Monitoring the MCU operating status using a watchdog timer [Window Watchdog function in the diagram]

- Monitoring signals that indicate abnormal MCU operation [MCU Hardware Failure Monitor function in the diagram]

- Control signals (such as reset signals) to transition the system to a safe state [Safety Outputs function in the diagram]

NXP's PMIC/SBC supports safety designs with the above features.

 

NXP Safety PMIC FS86NXP Safety PMIC FS86NXP Safety PMIC FS86


Advantage 2: Provides optimal power supply voltage and power supply startup sequence control

S32 microcontrollers have multiple power supply inputs (VCORE, VDDIO, VREF, etc.), and each needs to be supplied with the required voltage at the required timing. NXP's PMIC/SBC is equipped with OTP (One Time Programming) memory, which not only allows the on-board DCDC and LDO to supply the optimal output voltage and current to the S32 microcontroller's power input, but also allows you to set the power startup sequence (power-on order and timing) required for the S32 microcontroller.

This feature reduces the time and effort required for power supply design, shortening development time and helping to bring products to market quickly.

S32K3マイコン向けPMIC/SBC FS26 電源起動シーケンスS32K3マイコン向けPMIC/SBC FS26 電源起動シーケンスPMIC/SBC FS26 power supply startup sequence for S32K3 microcontrollers


Advantage 3: Low power consumption mode for efficient use of power

NXP's PMIC/SBC is equipped with a low-power consumption mode that is linked to the operating mode of the S32 microcontroller.

The PMIC/SBC can be transitioned from normal mode to low power consumption mode ( standby or low power mode ) by a control signal (via I²C/SPI ) from the S32 microcontroller, and the PMIC/SBC can be returned from low power consumption mode to normal mode by a wakeup signal.

By utilizing the PMIC/SBC's low-power modes, device standby current can be minimized, extending vehicle battery life.

PMIC/SBC 低消費電力モード遷移図PMIC/SBC 低消費電力モード遷移図PMIC/SBC low power consumption mode transition diagram


Benefit 4: NXP 's support for interoperability between microcontrollers and PMIC/SBCs

NXP's PMIC/SBC is included in the S32 microcontroller reference design and supports interoperability between the microcontroller and the PMIC/SBC .

Additionally, various documents are available to help you design a system that will work optimally.

Furthermore, with technical support from NXP and our distributors, we work with you to reduce development risks, including power supply design, software, and overall system support, allowing you to proceed with product development with peace of mind and contributing to early resolution of any problems that may arise.

S32K31XEVB-Q100 ボード リファレンスデザインS32K31XEVB-Q100 ボード リファレンスデザインS32K31XEVB-Q100 Board Reference Design


summary

As such, using NXP's PMIC/SBC together with an automotive microcontroller (S32 series ) offers many benefits. In particular, interoperability with NXP's S32 microcontrollers has been verified, enabling high-quality product development in a short period of time while minimizing the risks in power supply design.


Reference materials


=========================

We are currently unable to respond to comments in the "Comment" section of this post.
We apologize for the inconvenience, but when making inquiries, please refer to `` Technical Questions to NXP - How to Contact Us( Japanese Blog) ''.
(If you are already an NXP distributor or have a relationship with NXP, you may ask the person in charge directly.)

We will explain four benefits of using NXP's power management ICs (PMIC/SBC) with automotive microcontrollers (S32 series).

General Purpose MicrocontrollersintroductionPMICS32N ProcessorsS32Z|E ProcessorsJapanese blog
Tags (1)
No ratings
Version history
Last update:
‎11-23-2025 09:30 AM
Updated by: