2040537_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2040537_en-US

2040537_en-US

Extension update failled

 According to the document which named "Getting Started with MR-CANHUBK344 Evaluation Board", I tried to install about "S32K3 RTD AUTOSAR® 4.4 Version 2.0.0" and "S32K3xx development package Version 3.4.3". But it failed like an upload screenshot.
 Also I can't find "FreeRTOS for S32K3 2.0.0" at the extension list. How can install correctly?

Re: Extension update failled

Please refer to the offline installation and online installation methods mentioned in https://community.nxp.com/t5/S32K/S32K3-Unified-Bootloader-Build-Issue/td-p/1653130


S32K3 Reference Software -> Automotive SW - S32K3 - FreeRTOS -> SW32K3_FreeRTOS_10.4.6_2.0.0_D2204

Re: Extension update failledReason Details: Operation detailsYour original request has been modified."GNU ARM PEMicro Interface Debugging Support" is already installed, so an update will be performed instead.Software being installed: com.nxp.s32ds.brc.arm.tools.gcc102.feature.feature.group 1.0.0.202109281337 Missing requirement for filter properties ~= $0: com.nxp.s32ds.brc.arm.tools.gcc102.feature.feature.group 1.0.0.202109281337 requires 'org.eclipse.equinox.p2.iu; com.nxp.s32ds.brc.arm.tools.gcc102.feature.feature.jar [1.0.0.202109281337,1.0.0.202109281337]' but it could not be foundRe: Extension update failled" Also I can't find "FreeRTOS for S32K3 2.0.0" at the extension list. How can install correctly?" is solved.Re: Extension update failled

2.0.0 is no longer there. I only find 2.0.1 which doesn't work.

Can you point to SW32K3_FreeRTOS_10.4.6_2.0.0_D2204?

Tags (1)
No ratings
Version history
Last update:
‎05-30-2026 04:46 AM
Updated by: