2024641_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2024641_en-US

2024641_en-US

LPSPI_IP_BUSY state while transmitting data from Lpspi_Ip_AsyncTransmit() function

We have  an issue With S32k44,

configured LPSPI using EB tresos and tried to transmit data using Lpspi_Ip_AsyncTransmit()

call gets executed once Other calls are rejected because the drivers stay in the LPSPI_IP_BUSY state.

Can you please share an Example project of S32K344(with EB tresos configuration)

for Lpspi_Ip_AsyncTransmit(); using DMA?

#S32K344


Re: LPSPI_IP_BUSY state while transmitting data from Lpspi_Ip_AsyncTransmit() function

Thanks Petr

using this example I can use SPI, and the issue is resolved 

Re: LPSPI_IP_BUSY state while transmitting data from Lpspi_Ip_AsyncTransmit() function

Hi,

try to look over below example, not for EB but is using HLD driver as well.
https://community.nxp.com/t5/S32K-Knowledge-Base/Example-S32K344-SPI-Transmit-amp-Receive-Using-DMA-...
Also this one could be useful
https://community.nxp.com/t5/S32K/S32K344-SPI-DMA-with-MCAL-configuration-not-send-out-all-bytes/td-...

BR, Petr

标记 (1)
无评分
版本历史
最后更新:
‎11-21-2025 04:32 PM
更新人: