2017446_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2017446_en-US

2017446_en-US

Routing CAN and Ethernet pins using S32DS pin configurator
I'm trying to port the MR-CANHUB code to S32DS 3.6 + RTD 5.0.0 and ran into an issue with the CAN and Ethernet peripherals in the pin configurator.
 
The tool is telling me:
Issue: Incorrect assignment on 'Peripheral', 'Signal' items.
Level: Error
Type: Tool problem
Tool: Pins
Origin: Pins:PortContainer_0_BOARD_InitPeripherals
Resource: #102-FlexCAN_0.rxd
Information: ERRORS:
  – The selected peripheral is not supported for routing.
  – The FlexCAN_0 peripheral does not support routing.

---
 
I noticed the FlexCAN example from the RTD disables the pin configurator.
 
Do these need to be manually configured or are they supported by the pin configurator?
 
 
Re: Routing CAN and Ethernet pins using S32DS pin configurator

The pin names changed since the MR-CANHUB source was developed in RTD 2.0.0 and S32DS 3.4.

I was able to create new pin assignments for these and delete the originals. There are no longer any errors in the configurator.



タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 12:20 PM
更新者: