2014976_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2014976_en-US

2014976_en-US

Additional question for unused GPIO pins for SC16IS752

Would you please additionally confirm the existing post below?

SC16IS752 - what to do with unused pins - NXP Community

I would like to clarify the settings for unused GPIO0~GPIO7.

The previous post states output pin: floating, input pin: external pull-up or pull-down.

-Is this the same when used not only as GPIO0~GPIO7 but also as /DSRx, /DTRx, /CDx, and /RIx?

-About input pin, which is recommended, pull-up or pull-down?
  Is there a recommended resistance value?

Bata_0-1734417766500.png

Re: Additional question for unused GPIO pins for SC16IS752

Hi Rong

Sorry for my reply delay,

My question was cleared.

I appreciate that your answer.


Best regards,

Bata

Re: Additional question for unused GPIO pins for SC16IS752

Hi,

I suppose you are right.

For the unused pins, if the pin is an output pin, just have it float. If the unused pin is an input pin, connect it to a pull-up or pull-down resistor, the pull up/down resistor can be 10K ohm. Either pull-up or pull-down is okay, there is not different.

Hope it can help you

BR

XiangJun Rong


タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 04:37 PM
更新者: