SC16IS752 - what to do with unused pins

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SC16IS752 - what to do with unused pins

1,623 Views
jana_beck
Contributor II

Hello,
I could not find anything in the datasheet.
What is the best practice for unused pins for SC16IS752?

I currently do not need TXB, RXB, /RTSB, /CTSB and GPIO0 to GPIO7.

jana_beck_0-1611967235023.png

(I know a lot of unused pins, I am using this IC for another project already which makes it easier.)

Thanks!

0 Kudos
Reply
1 Reply

1,616 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Jana

I think it is a general guide for unused pins that the output pin can be float(No Connection), the input pin can be connected to external pull-up or pull-down resistor.

Hope it can help you

BR

XiangJun Rong

0 Kudos
Reply