2009165_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2009165_en-US

2009165_en-US

Industrial i.MX8QM clock frequencies

Hi everyone,

We are currently doing tests on the MIMX8QM5CVUFFAB and found some strange behaviour regarding clocks. The first thing we noted is that even though the clock is limited to 1.3 GHz for the Cortex A72 and 1.104 GHz for the Cortex A53, the cpufreq driver allows us to set the higher frequency of 1.6 GHz and 1.2 GHz. The SCFW seems to correctly ignore the higher frequencies but this leads to a missmatch between cpufreq and the actual clock rate:


root@apalis-imx8-15556460:~# cat /sys/bus/cpu/devices/cpu4/cpufreq/scaling_cur_freq
1596000
root@apalis-imx8-15556460:~# cat /sys/kernel/debug/clk/clk_summary |grep a72
 a72_clk                             0       0        0        1296000000  0          0     50000      Y   cpu4                            no_connection_id
root@apalis-imx8-15556460:~# cat /sys/bus/cpu/devices/cpu0/cpufreq/scaling_cur_freq
1200000
root@apalis-imx8-15556460:~# cat /sys/kernel/debug/clk/clk_summary |grep a53
 a53_clk                             0       0        0        1104000000  0          0     50000      Y   cpu0    

We would expect that this is either solved by a special cpufreq driver or then by a fdt fixup in U-Boot. However, I can't find any of this solutions in the BSP. Can you confirm that this is currently not implemented?

A second clocking issue affects the GPU, even though according to the datasheet the GPU should only run at 625 MHz it runs at 800MHz:


root@apalis-imx8-15556460:~# cat /sys/kernel/debug/gc/clk
gpu0 mc clock: 797983833 HZ.
gpu0 sh clock: 996002801 HZ.
gpu1 mc clock: 798002539 HZ.
gpu1 sh clock: 995989749 HZ.
root@apalis-imx8-15556460:~# cat /sys/kernel/debug/clk/clk_summary |grep gpu
 gpu_shader1_clk                     0       0        0        996000000   0          0     50000      Y   54100000.gpu                    shader
 gpu_core1_clk                       0       0        0        798000000   0          0     50000      Y   54100000.gpu                    core
 gpu_shader0_clk                     0       0        0        996000000   0          0     50000      Y   53100000.gpu                    shader
 gpu_core0_clk                       0       0        0        798000000   0          0     50000      Y   53100000.gpu

Here the SCFW does not limit the clock, which seems to be a violation of what is written in the datasheet. My expectation would also be here that there is a fdt fixup in U-Boot to address this but I could not find it. Can you confirm that this is currently not implemented?

The version of the SCFW, ATF and U-Boot should be recent enough to properly support the i.MX8QM with the 1.3 GHz limitation:


U-Boot 2024.04-34984-g64f00b21ff8 (Dec 04 2024 - 14:42:45 +0100)

CPU:   NXP i.MX8QM RevB A53 at 1104 MHz at 33C

DRAM:  4 GiB
Core:  203 devices, 24 uclasses, devicetree: separate
MMC:   FSL_SDHC: 0, FSL_SDHC: 1, FSL_SDHC: 2
Loading Environment from MMC... OK
In:    serial
Out:   serial
Err:   serial
Model: Toradex 0091 Apalis iMX8QM 4GB WB IT V1.1A
Serial#: 15556460
Boot:  MMC0
Reset cause: POR

 BuildInfo:
  - SCFW 83624b99, SECO-FW c9de51c0, IMX-MKIMAGE ca5d6b2d, ATF 616a458
  - U-Boot 2024.04-34984-g64f00b21ff8


Best regards,

Stefan

i.MX 8 Family | i.MX 8QuadMax (8QM) | 8QuadPlusLinuxRe: Industrial i.MX8QM clock frequencies

current bsp is based on nxp mek board, don't find specific bsp for industrial, you can change the bsp by yourself

Re: Industrial i.MX8QM clock frequencies

Hi @joanxie 

Thanks for the update. Can you point me to the right BSP for the industrial version of the i.MX8?

Thanks and best regards
Stefan

Re: Industrial i.MX8QM clock frequencies

the bsp you used isn't for industrial, so the A72 core define 1596000000 as max, you can remove

this from a72_opp_table: opp-table-1

linux-imx/arch/arm64/boot/dts/freescale/imx8qm.dtsi at lf-6.6.y · nxp-imx/linux-imx · GitHub

you also can refer to this workaround, for the 1.3G imx8qm 

[OUTDATED] Workaround for de-rating i.MX 8QM/QP parts before SCFW 1.16.0 releases - NXP Community


Re: Industrial i.MX8QM clock frequencies

Hi @joanxie 

The following versions are used:
SCFW: 1.17.0 (83624b99)
U-Boot: lf_v2022.04 https://github.com/nxp-imx/uboot-imx/tree/lf_v2024.04
Linux: lf-6.6.y https://github.com/nxp-imx/linux-imx/tree/lf-6.6.y

Regards,
Stefan

Re: Industrial i.MX8QM clock frequencies

what bsp version and SCFW version do you test? let me double check it

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎11-21-2025 12:40 PM
更新者: