Downloading S32_SDK_S32K1xx_RTM_4.0.3 in s32ds will give an error,If downloaded offline, S32_SDK_S32K1xx_RTM_4.0.3 cannot be found in the official website
Some companies' IT restricts http access, so it is recommended to change Available S32DS Software Sites to https.
So now I have returned s32ds 3.4, but can not find S32_SDK_S32K1xx_RTM_4.0.3
Do not use S32K1 SDK with S32DS v3.5. According to the currently available information, we don’t have any plan to integrate S32SDK S32K1XX 4.0.3 into S32DS 3.5 or above version.
I want to open the project created by old version s32ds3.4+S32_SDK_S32K1xx_RTM_4.0.3, I tried s32ds 3.5 does not work with old version project
Extensions and Updates install the S32 SDK for S32K1xx RTM 4.0.3 in S32DS 3.4.Prompts installation failure, like the first image,S32K1xx development package only S32K1 SDK 4.0.2,There is no S32 SDK for S32K1xx RTM 4.0.3
Hi
You should be able to use Extensions and Updates install the S32 SDK for S32K1xx RTM 4.0.3 in S32DS 3.4.
If the online installation fails, please install the S32K1xx development package first, and then install S32SDK S32K1XX RTM 4.0.3. Sorry, there is no offline installation package for S32K1 SDK 4.0.3.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------