1969446_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1969446_en-US

1969446_en-US

s32k3x4 -t172 debug error

why i am getting this error Capture.PNG

Re: s32k3x4-t172 debug errorI change probe its working fine thank youRe: s32k3x4-t172 debug error

I updated PEMicro software and S32DS Update 14 but still can't reproduce the problem you mentioned. Do you have other development boards? Also, do your colleagues encounter this problem?
In addition, from the ssb.PNG, I can see that the S32K3 RTD you installed is version 3.0.0 P01 instead of the RTD 5.0.0 you mentioned before.

PEMicro Interface Settings.pngdebug Pit_Gpt_Ip_Example_S32K344.png

Re: s32k3x4-t172 debug error

i already have all software installed  still i am getting an error message but for Dio example it works after trying 4 to 5 time but not for pother peripheral

Re: s32k3x4 -t172 debug error

I don't have this problem, please compare my Installation Details

S32K3 RTD 5.0.0 Installation Details.png

Re: s32k3x4 -t172 debug errorI am using only Onboard OPEN SDA debuggerRe: s32k3x4 -t172 debug errorversion for s32DS is 3.5
and RTD 5.0.0
yes
s32k3x4evb-T172 REV B2
I just check with open sda
Re: s32k3x4 -t172 debug error

Please tell me:
Which version of Update did you install for S32DS v3.5?
Which version of S32K3 RTD?
Did you update PEMicro Software?
Which S32K3 development board? S32K3X4EVB-T172 RevB or RevB2?
I have not encountered this problem with the onboard OpenSDA, only when using the external PEMicro Multilink.

Re: s32k3x4 -t172 debug error

i am not using external debugger its on board debugger only 

Re: s32k3x4 -t172 debug errorhow to configure and where to downloadRe: s32k3x4 -t172 debug error

Hi

It is recommended to use the onboard OpenSDA (J40) debugger.

Are you using an external PEMicro Multilink debugger? If so, please note:
"USB Multilink FX RevA and Universal Rev A and B are based on legacy UF32 USB devices, which are no longer actively supported/validated by PEmicro under the latest plugins/software packages.
To get latest support user would need Multilink FX Rev C, Multilink Universal Rev C/D or Multilink ACP"

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 08:23 PM
Updated by: