Hello,
I have been installed the HSE FW, and read HSE FW version succeed.
But when I program demo app again, I got a programming error as shown below picture, than I found the HSE installation state lost.
there are a total of 3 ECU with same problem. I don't know why. Is it possible for the HSE FW to be lost?
update to fix unclear picture
It looks like your S32K312's current SBAF Version(0x4039C020) is 01 0D 00 00 00 09 00 01. To make it fully compatible with SBAF, it is recommended to install HSE FW version 00 0D 00 00 02 06 00 00 or higher.
Which HSE_DEMOAPP are you using? HSE_DEMOAPP_S32K3XX_0_2_6_0 or the latest HSE_DEMOAPP_S32K3XX_0_2_40_0?
BTW, S32K312 SBAF 0.15.0 RTM Release is the latest version.
Hi
Sorry, there may be something wrong with the method you uploaded the picture, so I can't see the content of the picture clearly. Please click Insert Photo or attach those pictures.
Have you referred to MU Restore FW_EN.pdf in S32K312 HSE strange problem?
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------