1839261_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1839261_en-US

1839261_en-US

SDK is not showing

Installed S32DS V4,

as per manual installed the necessary SW,

During project creation unable to see the SDK


Followed the steps from the below document

RajCS_0-1712053543088.png

 #nxp S32G2 

Re: SDK is not showing

Hi,

It seems that this issues are the same as the community thread shown below:

S32G3 board ,unable to find the FSL image is not available in SD card - NXP Community

Information has been provided under the above community thread.

Please, let us know.

Re: SDK is not showing

HI @Daniel-Aguirre ,


There are 2 issues I'm facing.

I connected Micor USB cable to PC and J4 connector. USB is not detected.


RajCS_0-1713793736667.png

2)Build is incomplete


RajCS_1-1713793811989.png





Re: SDK is not showing

Hi,

Thanks for your feedback.

Can you help us share with us which RTD package have you installed? Are you able to see available examples under your setup? Which GCC version did you choose in the previous window?

Please, let us know.

Re: SDK is not showingHi @Daniel-Aguirre
I have tried same thing,but no luck. Pls let me know if you need any other details.
Re: SDK is not showing

Hi,

Can you help us share with us which RTD package have you installed? Are you able to see available examples under your setup? Which GCC version did you choose in the previous window? We can also recommend the following HOWTO on this same regard:

HOWTO: Create a Blinking LED application project for S32G using S32 RTD No AUTOSAR - NXP Community

Please, let us know.

Tags (1)
No ratings
Version history
Last update:
‎11-21-2025 04:24 PM
Updated by: